Hexavalent Chrome Removal From Drinking Water 

Hexavalent Chrome Removal From Drinking Water 

Water Technologies
Language
  • English
  • Deutsch
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Drinking Water Treatment
    • Aeration and Gas Stripping
    • Arsenic Removal
    • Chemical Feed and Control
    • Disinfection
    • Disinfection By-Products Removal
    • Dissolved Metals Removal
    • Fluoridation
    • Hexavalent Chrome Removal
    • Hydrogen Sulfide Removal
    • Iron and Manganese Removal
    • Mercury Removal
    • Perchlorate Removal
    • Softening - Hardness Removal
    • Taste and Odor Control
    • TOC Reduction
    • VOC Removal
    • Water Clarification and Filtration
    • Water Quality Analyzers and Process Control
  • Hexavalent Chrome Removal

Hexavalent Chrome Removal from Drinking Water

Though widely distributed in soil, chromium is not common in natural waters.  Rather, its presence occurs in surface waters as a result of improper wastewater treatment from electroplating, leather tanning, and textile industries.  Chrome contaminantion in waters destined for potable, drinking use creates some level of human health concerns ranging from very mild to severe and is dependent upon the level of concentration and exposure.

Ion Exchange Resins
Ion exchange provides an effective treatment option for chrome removal from surface waters

Many heavy metals, such as chrome, have been found in harmful concentrations in surface waters due to contamination introduced from industrial pollution.  Once present, chromium compounds are very persistent in water and often, are present in particulate form as sediment. Some of the particulate chromium will remain as suspended matter and ultimately be deposited in sediments.

Industrial use of chromium includes in metal alloys such as stainless steel; protective coatings on metal; magnetic tapes; and pigments for paints, cement, paper, rubber, composition floor covering and other materials. 

Increased urbanization and drinking water demand in areas of industrial activity has increased the frequency of problem metals in drinking water.  The presence of chrome in waters destined for potable drinking use have the potential to cause damage to liver, kidney, circulatory and nerve tissues and skin irritation from long-term exposures at levels above the Maximum Contaminant Level (MCL).  Currently, the US Environmental Protection Agency's (EPA) MCL in drinking water for chrome has been set at 0.1 parts per million (ppm).  The US EPA has designated the following treatment methods as Best Available Technology (BAT) for removing chromium from water.

Ion exchange is the most frequently used  treatment technology for chromium.  This technology removes chromium ions from the aqueous phase by replacing them with the anion present in the ion exchange resin.  As contaminated water is passed through the resin, contaminant ions are exchanged for other ions such as chlorides or hydroxides in the resin. 

Siemens Water Technologies offers both permanent, hard-piped systems as well as a potable ion exchange (PIX) service which features removable systems.  The PIX service approach integrates equipment and service option combinations, thereby minimizing capital investment and reducing overall space requirements.  The system vessels are selected based upon available manpower, space limitations, access limitation and the specific water quality required.  Depending on the contaminant to be removed and treated quality requirements, we choose the best media options from a variety of available ion exchange resins and other removal medias, such as activated carbon.  Potable ion exchange service provides the ultimate flexibility to add or remove treatment capacity as your business grows or compliance limits change.  If needs change, we can simply change the media types and/or tank size, thereby saving our customers significant capital expense.

Once exhausted, the exchange vessels are removed and replaced with fresh, potable-use vessels and returned to service.  The resins/activated carbon medias are removed from the site and delivered to a local resin regeneration facility for destruction and/or landfill

Potable service ion exchange minimizes the need for handling and on-site storage of chemicals and wastes for improved safety and compliance at your site. This option also saves valuable manufacturing space while minimizing your maintenance and installation requirements.

(Note:  Ion exchange is often preceded by treatments such as filtration to remove organics, suspended solids, and other contaminants that can foul the resins and reduce their effectiveness.)

Coagulation and/or filtration are alternative treatment technologies for chrome removal.  This technology consists of decreasing the pH level (as low as 4 or 5) and increasing the feed rate of a chemical coagulant combined with mechanical flocculation to allow fine suspended and some dissolved solids to clump together (floc). There are a variety of coagulants available (e.g. aluminum sulfate, ferric chloride, ferric sulfate, poly aluminum chloride, etc.), and the choice of one depends on water quality, contaminant removal requirements and cost. The majority of the floc and other suspended solids are removed by settling.

 

The remaining suspended particles are removed by filtration using multimedia filters. Water passes through the filtration media bed and the suspended solids are captured in the bed.  This continues until the bed has reached a maximum solids loading.  The flow is reversed causing bed expansion and release of the captured solids.

 

Filter backwash waste water and spent filtration medias all require special handling and disposal considerations which Siemens can provide assistance with.

 

Hexavalent Chrome Removal Treatment Technologies

Ion Exchange
Coagulation
Flocculation

top of page

Contact Us

For more information about chrome removal from drinking water, contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Hexavalent Chrome Removal from Drinking Water Case Study

Siemens Provides System and Services to Treat Hexavalent Chrome Contamination in Kansas Groundwater Supply for Public Drinking Water 

City of Colby, Kansas needed to treat chromate contaminated groundwater from the Ogalala drinking water aquifer.  Ace Services, a farm implement manufacturing company contaminated the groundwater from inappropriate discharge of their chroming process.  The company has since gone out of business and the project is now part of an EPA Superfund Cleanup.

Siemens’ design features once-through, single-use ion exchange resin technology.  The resulting treated water is pumped directly to the City of Colby potable water system.


Read the full case study

Hexavalent Chrome Removal Case Study
top of page
Print
Contact Us

Featured Hexavalent Chrome Removal Products and Services

Ion Exchange Systems
Ion Exchange Medias
Activated Carbon Medias
Potable Ion Exchange (PIX) Service 

Featured Case Study

Siemens Provides System and Services to Treat Hexavalent Chrome Contamination in Kansas Groundwater Supply for Public Drinking Water 

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID