Hexavalent Chrome Removal from Groundwater 

Hexavalent Chrome Removal from Groundwater 

Water Technologies
Language
  • English
  • Deutsch
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Groundwater Remediation
    • Arsenic Removal
    • Chemical Feed and Control
    • Dissolved Metals Removal
    • Hexavalent Chrome Removal
    • Iron & Manganese Removal
    • Landfill Leachate Treatment
    • Nitrate Removal
    • Organic Chemicals Removal
    • Perchlorate Removal
    • VOC Removal
    • carbon-treat-contaminated-wells
    • pv-varbon-rainwater-runoff
  • Hexavalent Chrome Removal

Hexavalent Chrome Removal from Groundwater

Though widely distributed in soil, chromium is not common in natural waters.  Rather, its presence occurs in surface waters as a result of improper wastewater treatment from electroplating, leather tanning, and textile industries.  As with other metals,  in cases where the groundwater is destined for potable use, chrome contaminantion creates some level of human health concerns ranging from very mild to severe.

Ion Exchange Resins
Ion exchange provides an effective treatment option for removal of chrome from groundwaters

Many heavy metals, such as chrome, have been found in harmful concentrations in surface waters due to contamination introduced from industrial pollution.  Once present, chromium compounds are very persistent in water and often, are present in particulate form as sediment. Some of the particulate chromium will remain as suspended matter and ultimately be deposited in sediments.

Industrial use of chromium includes in metal alloys such as stainless steel; protective coatings on metal; magnetic tapes; and pigments for paints, cement, paper, rubber, composition floor covering and other materials. 

Increased urbanization and drinking water demand in areas of industrial activity has increased the frequency of problem metals in drinking water.  The presence of chrome in groundwaters destined for potable drinking water applications have the potential to cause damage to liver, kidney, circulatory and nerve tissues and skin irritation from long-term exposures at levels above the Maximum Contaminant Level (MCL).  Currently, the US Environmental Protection Agency's (EPA) MCL in drinking water for chrome has been set at 0.1 parts per million (ppm).  The US EPA has designated the following treatment methods as Best Available Technology (BAT) for removing chromium from water.

Ion exchange is the most frequently used treatment technology for chromium.  This technology removes chromium ions from the aqueous phase by replacing them with the anion present in the ion exchange resin. As contaminated water is passed through the resin, contaminant ions are exchanged for other ions such as chlorides or hydroxides in the resin. 

Siemens Water Technologies offers a service-based treatment option for handling hexavalent and trivalent chrome contamination. For non-potable applications, our Wastewater Ion Exchange (WWIX) approach integrates equipment and service option combinations, thereby minimizing a plant’s capital investment and reduces overall space requirements.  The system vessels are selected based upon available manpower, space limitations, access limitation and the specific water quality required.  Based on the particulars of the contaminant to be removed and inlet quality requirements, we have access to a variety of ion exchange resins and other removal medias, such as activated carbon.  Wastewater Ion Exchange provides the ultimate flexibility to add or remove treatment capacity as your business grows or compliance limits change.  If needs change, we can simply change the media types and/or tank size, thereby saving our customers significant capital expense.

Once exhausted, the exchange vessels are removed and replaced with fresh, DOT-compliant vessels and returned to service. For non-potable applications, exhausted vessels are transferred to our central treatment and processing facility where the hazardous/non-hazardous contaminants are removed from the media/resin for reuse. 

For waters destined for potable use and drinking water applications, Siemens offers Potable Ion Exchange (PIX) Service.  PIX utilizes potable ion exchange resin canisters for the removal of organic and inorganic contaminants in surface and groundwater sources to meet drinking water standards. Each application is examined to determine the system configuration that best meets current and future needs.  Once the treatment media is spent, or reaches the end of it's useful life, the potable canisters are removed from the site and delivered to a local regeneration facility for destruction and/or landfill.

Both WWIX and PIX minimize the need for handling and on-site storage of chemicals and wastes for improved safety and compliance at your site. This option also saves valuable manufacturing space while minimizing your maintenance and installation requirements.
(Note:  Ion exchange is often preceded by treatments such as filtration to remove organics, suspended solids, and other contaminants that can foul the resins and reduce their effectiveness.)

Coagulation and/or filtration are alternative treatment technologies for chrome removal.  This technology consists of decreasing the pH level (as low as 4 or 5) and increasing the feed rate of a chemical coagulant combined with mechanical flocculation to allow fine suspended and some dissolved solids to clump together (floc). There are a variety of coagulants available (e.g. aluminum sulfate, ferric chloride, ferric sulfate, poly aluminum chloride, etc.), and the choice of one depends on water quality, contaminant removal requirements and cost. The majority of the floc and other suspended solids are removed by settling.

 

The remaining suspended particles are removed by filtration using multimedia filters. Water passes through the filtration media bed and the suspended solids are captured in the bed.  This continues until the bed has reached a maximum solids loading.  The flow is reversed causing bed expansion and release of the captured solids.

 

Filter backwash waste water and spent filtration medias all require special handling and disposal considerations which Siemens can provide assistance with.

 

Hexavalent Chrome Removal Treatment Technologies

Ion Exchange
Coagulation
Flocculation

top of page

Contact Us

For more information about chrome removal from groundwater, contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Hexavalent Chrome Removal from Groundwater Case Study

Hexavalent Chrome Contamination in Texas Groundwater Treated by Wastewater Ion Exchange Service

In 2003, Siemens Water Technologies was awarded a contract to provide design, installation and off-site recovery for a chromate contaminated groundwater supply in Odessa, Texas.  The site was the previously home to a number of chrome plating shops that had since gone out of business.

Read Full Case Study

Hexavalent Chrome Removal Case Study
top of page
Print
Contact Us

Featured Hexavalent Chrome Removal Products and Services

Ion Exchange Systems
Ion Exchange Medias
Activated Carbon Medias
Wastewater Ion Exchange (WWIX) Service
Potable Ion Exchange (PIX) Service
Hazardous/Non-Hazardous Waste Treatment and Recycling Service

Featured Case Studies

Hexavalent Chrome Contamination in Texas Groundwater Treated by Wastewater Ion Exchange Service
Siemens Provides System and Services to Treat Hexavalent Chrome Contamination in Kansas Groundwater Supply for Public Drinking Water 

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID