Hexavalent Chrome Removal from Wastewater 

Hexavalent Chrome Removal from Wastewater 

Water Technologies
Language
  • English
  • Deutsch
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Wastewater Treatment
    • Alkaline Cleaner Recovery
    • Archimedes / Screw Pumping
    • Biological Treatment
    • BOD & COD Reduction
    • Chemical Feed and Control
    • Clarification and Sedimentation
    • Disinfection
    • Dissolved Metals Removal
    • Hazardous Waste Treatment
    • Hexavalent Chrome Removal
    • Nutrient Removal
    • Oil and Water Separation
    • Primary Treatment
    • Secondary Treatment
    • Spent Caustic Treatment
    • Tertiary Treatment
    • TOC Reduction
    • Water Quality Analyzers and Process Control
  • Hexavalent Chrome Removal

Hexavalent Chrome Removal from Wastewater

Many manufacturing processes, such as those used by the electroplating, leather tanning, and textile industries produce wastewaters containing chromium.  The US Environmental Protection Agency has established standards that require the destruction of chromates prior to discharge to avoid the potential risks of surface and drinking water contamination.  In reuse applications, chrome is removed to meet the specific makeup water needs of the application. 

Ion Exchange Resins
Ion exchange provides an effective treatment option for removal of chrome from wastewater

Many heavy metals, such as chrome, have been found in harmful concentrations in surface waters due to contamination introduced from industrial pollution.  Once present, chromium compounds are very persistent in water and often, are present in particulate form as sediment. Some of the particulate chromium will remain as suspended matter and ultimately be deposited in sediments.

Industrial use of chromium includes in metal alloys such as stainless steel; protective coatings on metal; magnetic tapes; and pigments for paints, cement, paper, rubber, composition floor covering and other materials. 

Increased urbanization and the drinking water demand in areas of industrial activity has increased the attention paid to this problem metal.  Improper handling and or discharge into local sewers and the environment createst the potential for contamination of drinking water sources.  The presence of chrome in potable drinking water sources has the potential to cause damage to liver, kidney, circulatory and nerve tissues and skin irritation from long-term exposures at levels above the Maximum Contaminant Level (MCL).  Currently, the US Environmental Protection Agency's (EPA) MCL in drinking water for chrome has been set at 0.1 parts per million (ppm). 

Additionally, removal of chrome from wastewater is also needed to achieve the water quality level needed for reuse and recycling.  Many industries are turning to reuse and recycling practices to reduce the cost and volume of makeup water.

The US EPA has designated the following treatment methods as Best Available Technology (BAT) for removing chromium from water.

Ion exchange is a frequently used  treatment technology for chromium removal.  This technology removes chromium ions from the aqueous phase by replacing them with the anion present in the ion exchange resin.  As contaminated water is passed through the resin, contaminant ions are exchanged for other ions such as chlorides or hydroxides in the resin. 

Siemens Water Technologies offers both permanent, hard-piped systems as well as service-ion exchange which features removable systems.  Our service ion exchange approach integrates equipment and service option combinations, thereby minimizing a plant’s capital investment and reducing overall space requirements.  The system vessels are selected based upon available manpower, space limitations, access limitation and the specific water quality required.  Based on the application (potable vs. non-potable), contaminant to be removed and quality requirements, we have access to a variety of ion exchange resins and other removal medias, such as activated carbon.  Service ion exchange provides the ultimate flexibility to add or remove treatment capacity as your business grows or compliance limits change.  If needs change, we can simply change the media types and/or tank size, thereby saving our customers significant capital expense.

Once exhausted, the exchange vessels are removed and replaced with fresh, DOT-compliant vessels and returned to service. For non-potable applications, exhausted vessels are transferred to our central treatment and processing facility where the hazardous/non-hazardous contaminants are removed from the resin prior to disposal or reuse.  For potable applications, the resins are removed from the site and delivered to a local resin regeneration facility for thermal destruction and disposal.  Alternatively, single-use, non-regenerable ion exchange resins may also be used. 

Service ion exchange minimizes the need for handling and on-site storage of chemicals and wastes for improved safety and compliance at your site. This option also saves valuable manufacturing space while minimizing your maintenance and installation requirements.

(Note:  Ion exchange is often preceded by treatments such as filtration to remove organics, suspended solids, and other contaminants that can foul the resins and reduce their effectiveness.)

Wastewater discharge compliance is also achieved by reducing hexavalent chromium to trivalent chromium with precipitation to chromium hydroxide, a non-toxic substance.  Coagulation and/or filtration technology consists of decreasing the pH level (as low as 4 or 5) and increasing the feed rate of a chemical coagulant combined with mechanical flocculation to allow fine suspended and some dissolved solids to clump together (floc). There are a variety of coagulants available (e.g. aluminum sulfate, ferric chloride, ferric sulfate, poly aluminum chloride, etc.), and the choice of one depends on water quality, contaminant removal requirements and cost. The majority of the floc and other suspended solids are removed by settling and easily separated and disposed of.

The remaining suspended particles are removed by filtration using multimedia filters. Water passes through the filtration media bed and the suspended solids are captured in the bed.  This continues until the bed has reached a maximum solids loading.  The flow is reversed causing bed expansion and release of the captured solids.

 

Filter backwash waste water and spent filtration medias all require special handling and disposal considerations which Siemens can provide assistance with.

 

Hexavalent Chrome Removal Treatment Technologies

Ion Exchange
Coagulation
Flocculation

top of page

Contact Us

For more information about chrome removal from wastewater, contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Hexavalent Chrome Removal from Wastewater Case Study

Parker Hannifin, Formerly Aeroquip, Complies With Local Pretreatment Regulations Using Microfiltration, Dewatering, and Drying Equipment

Located in New Haven, Indiana, the new facility was built in 1992 to manufacture brass air compressor fittings for automobiles and appliances.  Before approximately 165 gpm of wastewater could be discharged, it needed to be treated for the removal of chromium, copper, lead and zinc.

Read More

Hexavalent Chrome Removal Case Study
top of page
Print
Contact Us

Featured Hexavalent Chrome Removal Products and Services

Ion Exchange Systems
Ion Exchange Medias
Wastewater Ion Exchange Service
Hazardous/Non-Hazardous Waste Treatment and Recycling Service

Featured Case Studies

Parker Hannifin, Formerly Aeroquip, Complies With Local Pretreatment Regulations Using Microfiltration, Dewatering, and Drying Equipment
Hexavalent Chrome Treatment for Rinsewater Recycling Reduces Feedwater Demand and Wastewater Discharge

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID