Rainwater Harvesting 

Rainwater Harvesting 

Water Technologies
Language
  • English
  • Deutsch
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
    • Siemens at Singapore International Water Week 2012
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Water Recycle & Reuse
    • Chemical Feed and Control
    • Disinfection
    • Industrial Water Recycle
    • Municipal Wastewater Reuse
    • Rainwater Harvesting
    • Wastewater Reclaim and Reuse
    • Water Quality Analyzers and Process Control
    • Advanced Membrane Filtration for Water Reuse Applications
    • Albert Köhler - Gengenbach, Germany
  • Rainwater Harvesting

Rainwater Harvesting

Many communities and industries are facing water shortages, deteriorating water quality and greater demands due to population growth, tourism, recreational use, drought and industrial expansion.  One method of combating water shortages and reducing demand on potable water is rainwater harvesting.  Our total solutions approach has helped universities, large office buildings, commercial and retail buildings to reduce demand on potable water by up to 40% using specially designed rainwater collection and treatment systems.

 

Depending on the size, or flow rate, of the rainwater harvesting system, and the intended use of the reclaimed water, these systems will vary in design and complexity.  Rainwater harvesting systems reduce potable water consumption typically used for non-potable applications such as toilet and urinal flushing, laundry and irrigation.  Only under ideal conditions (lots of rain and very little non-potable water requirements) will rainwater harvesting replace potable water for non-potable applications.

pH Control Skid

Very simply, rainwater harvesting systems are comprised of the following:

1. Collection

2. Treatment

3. Storage

4. Distribution

 


Collection
of rainwater and other condensation sources such as air conditioning units is the first step in the process.  This consists of a simple array of piping, troughs or ducts to collect the water sources and direct them to a storage tank, reservoir or cistern.  As the water enters the storage, it is filtered to remove debris.

 

Bag filters are often used here due to their high capacity, simplicity and low operating costs.

 Bag Filters

 

Treatment of the water begins with filtration typically in the 5 micron range.  From there, the water undergoes disinfection to eliminate microbiological substances such as bacteria, viruses and cysts.
 

Cartridge filters are the usual choice here. They can reliably remove minute particles and they occupy less space than bag filters for the same flow rate.

Cartridge Filters

Filter Housings

 

Disinfection methods can range from chemicals such as sodium hypochlorite or chlorine dioxide (both generated on site) to a chemical-free alternative such as ultraviolet (UV) light.  For small systems, UV light may be the only disinfection step.  A combination of chemical disinfection and UV disinfection are employed for larger systems.

UV Light Systems

On-Site Hypochlorite Generation Systems

Chlorine Dioxide Generation Systems

 

Depending on the source of the collected water, the pH or alkalinity of the water may need adjustment to prevent corrosion of the existing plumbing system and fixtures.  For this, a small chemical feed system is used to dose the appropriate chemical(s) to bring the water quality into alignment.  In some cases, a dye is added to the reclaimed water so that it is easily identified as being a non-potable source.

Chemical Feed Systems

 

Treatment systems must also include on line measurement and control ensuring safe, reliable and cost effective operation.  Even though the reclaimed water will not be used for potable applications, there is still a level of quality that must be maintained for safety and to meet regulatory guidelines.  In addition, precise measurement and control will ensure the lowest possible operating costs, reducing excess chemical and energy consumption.

Strantrol® 890 Controller
More Analyzers and Controllers

 

Storage of the treated water involves provisions for introduction of potable water to maintain the volume required for the demand.  As described earlier, reclaimed water will only reduce the amount of potable water for non-potable applications, not eliminate it.

 

For large storage tanks, it is common to circulate treated water through the storage tank and the disinfection system to maintain the desired level of residual disinfectant.  For smaller storage tanks, circulation is not necessary.

 

Distribution of the reclaimed water is the last step of the process.  Pumps deliver the water, through dedicated piping and plumbing, to the bathroom fixtures, laundry or irrigation system.  In some cases, UV light is used as a final disinfection step as the water is pumped from the storage tank for added safety.

Watch our Video to Learn More

Siemens Video

top of page

Contact Us

For more information on rainwater harvesting, contact the Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com

top of page

Rainwater Harvesting Case Study

Environmentally Friendly Modernization Project Reduces Water Consumption by 40% and Energy Consumption by 45%

In 2002, Portland State University (PSU) started a project for the environmentally friendly modernization of its buildings in order to reduce long-term costs and contribute to environmental protection. Siemens Water Technologies supplied them with an efficient rainwater reuse system to do so.

Read Full Case Study

Rainwater Reuse Case Study
top of page
Print
Contact Us

Featured Rainwater Harvesting Products

Filtration

Bag Filters

Cartridge Filters
Filter Housings

 

Disinfection

UV Light

On-Site Hypochlorite

Chlorine Dioxide

 

Chemical Feed systems
Metering Pumps

 

Analyzers and Controllers

Strantrol 890

More Analyzers and Controllers

Rainwater Harvesting Case Studies

Environmentally Friendly Modernization Project Reduces Water Consumption by 40% and Energy Consumption by 45%
Medical University in Atlanta, GA Chooses Siemens for its Water Reclaim System

Featured Article
From Grey to Blue
Article appeared in Engineering Design & Construction, August 2010

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID