key visual
site identifier
SIEMENS ARROW siemens.com 
country identifier
Home  |   Solutions  |  Products & Services  |  Parts & Support  |  About Us
Site Map  |   Contact Us
[Advanced]

Environmental Remediation

Capabilities
Technologies
Products
Services
Case Studies
Literature
Contacts


 
Groundwater Remediation News Releases

Results 1 to 10 of 20

05/09/2008|Processing Line for Stainless Steel: Posco orders special equipment and electrical systems from Siemens
Siemens Metals Technologies has received an order from Pohang Iron and Steel Company Ltd. (Posco) to supply special equipment, drives and the automation system for a cold-strip annealing, pickling and finishing line at the company's Pohang plant. The volume of the project is in the two-digit million Euro range. The new equipment is intended for the processing of stainless steel strips and is scheduled to start production in the middle of 2009.
 More
05/08/2008|Siemens Supplies Gearless Mill Drives for Aurox Iron-Ore Project in Western Australia
The Siemens Industry Solutions Division has received an order from Aurox Resources Ltd., an Australian company based in Perth, to supply “Simine Mill GD” gearless drives for two ore mills which are part of the Balla-Balla iron-ore project in Western Australia. The two mills are to be equipped with “frozen charge shakers” which allow the controlled removal of charge stuck to the sides of the grinding pipe. The order has a volume of more than 20 million euros and the project is scheduled for completion in the third quarter of 2010.
 More
05/08/2008|Siemens Equips New Processing Line for BlueScope Indonesia
Siemens Metals Technologies has received an order from PT BlueScope Steel, Indonesia, to equip a new integrated zinc-coating and painting line. The processing line will be installed at the Cilegon site and is designed for an annual production of 175,000 metric tons of Zincalume® steel. The order value is in the two-digit million Euro range. The new facility is scheduled to start operating in the spring of 2010.
 More
05/06/2008|Efficient Extraction of By-Products for Sale to the Market – Siemens Modernizes Coke-Oven By-Product Plant at Isdemir, Turkey
A project comprising the expansion and modernization of a coke-oven by-product plant, which Siemens Metals Technologies implemented for the Turkish steel producer Isdemir, was completed in February 2008. Two semi-separate gas-treatment lines are now in operation, increasing the processing capacity from 70,000 to 140,000 Nm3 of coke-oven gas per hour. This allows Isdemir to extract and sell approximately 40,000 tons t/a of ammonium sulfate, 75,000 t/a of tar and 30,000 t/a of benzol. At the same time, environmental emissions are significantly reduced. The process automation supplied by Siemens enables plant monitoring and operating functions to be carried out from a central control pulpit. Precise monitoring and process control ensures that the plant achieves highest efficiency at a high level of quality control and operational safety.
 More
05/05/2008|The new SFC series: systematic measuring and controlling
The flexible SFC devices from Siemens Water Technologies constitute a new measuring and controlling series which complements the concept of the multi-functional MFC system. The SFC series is intended for single measurements of water parameters as is necessary in simple applications. One main function is controlled chemical dosing which is used when disinfectant has to be added, for example. The series of devices matches the MFC system not only in terms of design and dimensions but also in terms of the range of functions. The two types of device are based on the same software and can therefore be combined and communicate with each other via a CAN bus.
 More
04/30/2008|Network Analysis and Simulation in Profinet Networks: Siemens Develops New Solutions for Real-time Ethernet Applications
The Bany PNIO network analyzer and the Simba PNIO module in the Simit simulation system supplied by the Siemens Industry Solutions Division provide operators of Profinet networks with a number of new tools for efficient monitoring and simulation. Bany PNIO enables reaction-free real-time analysis of data traffic at rates of up to one gigabit per second and a resolution of ten nanoseconds. Simba PNIO simulates up to 256 devices on the controller in real time. Mixed operation of real and simulated devices is also possible, which makes it easier to expand facilities and accelerates their commissioning.
 More
04/30/2008|Siemens Rolling Mill Equipment Will Increase Productivity and Improve Product Quality at Nikkei Siam Aluminium
Siemens Metals Technologies has been awarded an order by Nikkei Siam Aluminium Ltd., Thailand, to modernize the company's aluminum rolling mill by supplying new mechanical equipment, as well as process and drive systems. This is intended to both increase productivity and further improve product quality to cope with the growing demand of automotive related industries. The new equipment will more than double both the rolling speed and the coil weight. This project has a total value of some 5.5 million euros, and is scheduled to be completed by the beginning of 2009.
 More
04/25/2008|Siemens to Modernize Aluminum Cold Rolling Stand for Alunorf
Siemens Metals Technologies has received an order from Aluminium Norf GmbH (Alunorf), Neuss, to modernize cold rolling stand No. 4. The scope of supply consists of the basis automation (including the technological controls), the process automation system, the power units of the drives and the digital drive controllers. Siemens is also responsible for all the installation work and for commissioning. Modification will start as early as 2008 and will be completed in December 2009.
 More
04/23/2008|Siemens to Supply Filtration and Produced Water Treatment System for Su Tu Vang Central Processing Platform, Offshore Vietnam
J. Ray McDermott Asia Pacific Pte Ltd (JRMAP) has selected Siemens Water Technologies to provide filtration and produced water treatment systems to the new Su Tu Vang CPP (Central Processing Platform) to be operated by the Cuu Long Joint Operating Company, offshore Vietnam. The order amount is US$ 4.6M. The filtration system will include fine and coarse filters that will be included in a seawater injection system for the removal of particulates. The produced water treatment system will include a skim vessel, hydrocyclones and dissolved gas flotation (DGF) equipment to treat produced water to meet discharge limitations. Project completion is scheduled for the fourth quarter of 2008.
 More
04/18/2008|Higher Productivity with Reduced Environmental Emissions – Start-up of Modernized Finger-Shaft EAF at Stahl Gerlafingen, Switzerland
In January 2008, the modernized finger-shaft electric arc furnace (EAF) of Stahl Gerafingen AG (part of the Beltrame Group) was restarted following a project duration of ten months and a furnace downtime of slightly more than three weeks for disassembly, erection and commissioning activities. The objective of this modernization, carried out by Siemens Metals Technologies, was to increase productivity and at the same time to reduce the emissions of the steel works which is located in the midst of the town of Gerlafingen. The EAF was equipped with a new shaft which included scrap-retaining fingers for the scrap preheating as well as an improved offgas exhaust system and an optimized charging process. The contractual performance parameters were met within a week. The capacity of the modernized furnace was increased considerably and the availability of the plant exceeded 98 percent within just a few weeks after commissioning.
 More
12Next >





Contact Us Print

©  Siemens AG 2008 - Water Technologies, Corporate Information | Privacy Policy | Terms of Use | Digital ID