SIEMENS

 

Products 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
      • Contact Us
      • Request A Proposal
    • Municipal
      • Drinking Water
      • Remediation
      • Residuals Management
      • Wastewater
      • Water Reuse and Desalination
    • Wastewater
      • Products
      • Services
      • Case Studies
      • News Releases
      • WEFTEC 2009
    • Products

    Wastewater - Products

    Results 1 to 10 of 202

    The Trans-Flo® Secondary Clarifier - Three Proven

    Technologies in One

    The Trans-Flo® Secondary Clarifier has combined three proven technologies - The Rim-Flo® Peripheral Feed and Takeoff Clarifier, the Tow-Bro® Hydraulic Sludge Remover and the Chain & Scraper Sludge Collection System to assure a fresher, more concentrated sludge, reduced aeration requirements and lower effluent solids.  More

    Acutec™ 35 Gas Detector
    Acutec 35 Gas Detection System utilizes the latest on-line gas monitoring technology to provide a flexible and reliable, self testing detection system in a compact, modular design. Acutec 35 is ideal for detecting leaks from storage containers, process piping or gas feed equipment in any type of water, wastewater or industrial plant environment.  More

    AGAR® (Attached Growth Airlift Reactor) Biological Treatment System

    Using the AGAR® biological treatment system you can expand an existing wastewater treatment plant's capacity by nearly 100%, improve water quality to meet the most stringent requirements and even construct a new plant with a footprint as small as a 1/4 that of a traditional activated sludge process.

     

     More

    AquaCarb® S Granular Reactivated Carbons
    AquaCarb® S Series carbons are produced through thermal reactivation of approved grades of spent carbon at one of our state-of-the-art reactivation facilities.  More

    Aqua-Lator® Surface Aerators
    The Aqua-Lator® surface aerator is a floating mechanical aerator for wastewater treatment providing oxygen transfer, mixing and dispersion.  More

    Aqua-Lator™ Direct Drive Mixers (DDM)
    The Aqua-Lator™ DDM uses a powerful downward propeller driven pumping action without introducing any additional oxygen into the wastewater. The mixer helps to disperse oxygen into an aeration basin, pond or lagoon and keeps solids in suspension for optimal biological activity.  More

    Aqua-Lator™ Floating Spray Coolers
    Breaks up process water or wastewater into small particles so there is more surface area in contact with the ambient air, thereby increasing heat transfer and cooling  More

    Aqua-Scrub™ Low Pressure Liquid Phase Adsobers
    The Aqua-Scrub™ series carbon adsorbers are designed for use as a temporary or permanent treatment step in a variety of low flow and low pressure water treatment applications.  More

    AQUIT® Solution for Odor and Corrosion Control
    AQUIT® solution provides cost effective odor and corrosion control by preventing the formation of dissolved hydrogen sulfide in the collection system and downstream of the treatment facility.   More

    Arsenic Removal with GFH® Media
    GFH ferric-based media is used in an adsorption process to remove arsenic and other heavy metals from treated wastewater and drinking water supplies. Pre-oxidation is not required for arsenic removal applications. Once the media has exhausted its adsorption capacity, it is removed from the vessel and replaced with new media. The simplicity of this process with single use media is very attractive for small installations and wellhead applications especially where no treatment currently exists.  More

    12345678910Next >
    top of page
    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID