key visual
site identifier
SIEMENS ARROW siemens.com 
country identifier
Home  |   Solutions  |  Products & Services  |  Parts & Support  |  About Us
Site Map  |   Contact Us
[Advanced]

Industrial Wastewater Systems

Capabilities
History
Products
Services
Case Studies
Brochures
Contacts
Locations and Directions

Water Technologies > Product and Service Lines > Industrial Wastewater Systems > Products

 
Flue Gas Desulfurization

Siemens Water Technologies offers a complete treatment solution for flue gas desulfurization (FGD) wastewater, ensuring that power plants meet Phase 2 of the Clean Air Act amendments.

This solution includes engineering design, equipment supply, installation, checkout, startup, commissioning, operation, maintenance, financing or build-own-operate-maintain (BOOM) / build-own-operate-transfer (BOOT).

Features and Benefits

We combine several proven technologies to achieve a well functioning, integrated FGD treatment facility with appropriate performance guarantees, including:

  • Lime neutralization / desaturation
  • Heavy metal removal, including hard-to-remove priority species
  • Clarification
  • Filtration
  • Sludge thickening and dewatering
  • BOD / COD reduction
  • Nitrates and ammonia reduction

Scrubber Technology

 

Scrubbers are used in U.S. power plants to meet air quality emission standards set by the U.S. Environmental Protection Agency (EPA) and by individual state requirements.  Recent updates to the regulatory programs call for further reduction of sulfur dioxide (SO2) emissions from coal-burning power plants.

FGD systems use either dry or wet scrubbers. Dry scrubbers generally use lime or limestone as a reagent to remove SO2 and although they use water in the process, the water usage is lower than with wet scrubbers. When the power plant's coal contains less than 2% sulfur, as it does in western coals such as the Power River Basin (PRB) coal, the plant will typically consider using dry scrubbers. Wet scrubbers are preferred when the coal contains higher amounts of sulfur. Since a power plant being retrofitted with a new FGD system will be in service for 25+ years, a number of power plants are installing wet scrubbers, even if they are currently using low sulfur coal, to have the future flexibility to use coals from many different world sources that may have higher sulfur content.

Wet FGD systems most commonly are of the limestone-forced-oxidation (LSFO) type to convert SO2 in the flue gas to carbon & oxide. While this allows greenhouse gases to be released to the atmosphere, it removes the SO2 that causes acid rain.  Future versions of FGD systems will capture CO2 and dispose of it in an environmentally-friendly way.

Wet FGD scrubbers use an absorber tower in which flue gas is contacted by the limestone slurry, resulting in conversion of SO, in the flue gas into calcium sulfate (gypsum), with carbon dioxide (CO2) going up the stack. To maintain required conditions in the scrubber (to control chlorides levels consistent with the scrubber’s materials of construction and to maintain ash fines levels low enough to maintain gypsum quality), a constant purge stream is discharged from the scrubber system.

Flue gas systems frequently use limestone-forced-oxidation (LSFO) scrubbers to convert SO2 in the flue gas to gypsum, which can be sold to wallboard manufacturers, thus turning a waste stream into a usable resource.

The proper design of sludge dewatering systems and the selection of materials of construction are critical in FGD wastewater installations. Both of these key design areas can have a major impact on the treatment plant’s operation, reliability and cost.  Siemens Water Technologies has extensive expertise in FGD wastewater treatment and is the industry leader.  By having early discussions with the utility about their specific power plant, we are able to provide an optimized system at the best cost / benefit ratio.

Product Documentation


Featured Article

Read the article published in the January/February 2007 Edition of INDUSTRIAL WATERWORLD.
Treating FGD Wastewater: Phase 2 Clean Air Act Admenments Make it Hot Topic

Brochure
Flue Gas Desulfurization Wastewater Treatment



Contact Us

Brian Heimbigner
Business Development Manager
678.446.5273
Send email
Request a Proposal
Parts & Services

General Contact
2000 Marconi Drive
Warrendale, PA 10586
800.541.8610
iwsezservice.water@siemens.com

Featured News Releases

Allegheny Energy - Siemens to supply system for treating FGD wastewater.

Springdale, Pa.- Siemens to supply system for treating FGD wastewater.

Contact Us Print

©  Siemens AG 2008 - Water Technologies, Corporate Information | Privacy Policy | Terms of Use | Digital ID