SIEMENS

 

Chlorine Dioxide Removes Disinfection By-Product (DBP) Precursors at Rocky Mountain Municipality 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
      • Contact Us
      • Request A Proposal
    • Applications
      • Aquatic Water Treatment
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
    • Drinking Water Treatment
      • Arsenic Removal
      • Disinfection
      • Disinfection By-Products Removal
      • Dissolved Metals Removal
      • Fluoridation
      • Hexavalent Chrome Removal
      • Iron and Manganese Removal
      • Perchlorate Removal
      • TOC Reduction
      • VOC Removal
      • Water Clarification and Filtration

    Chlorine Dioxide Removes Disinfection By-Product (DBP) Precursors at Rocky Mountain Municipality

    Challenge

    This municipality disinfects 1-1.5 million gallons per day of drinking water, and is currently transitioning from a small system serving <10,000 people to a large system serving >10,000 people. Chlorine gas was used as the primary disinfectant for the raw water entering the plant. TTHM’s levels consistently averaged 64 μg/L, the trigger limit for disinfection profiling. HAA5’s averaged 48 μg/L, and TOC reduction was consistently between zero and the required removal rate of 25%. Reducing the levels of TTHM’s, HAA5’s and TOC and meeting compliance standards for both the Stage 1 D/BPR and the LT1 Enhanced Surface Water Treatment Rule prompted the municipality to consider different pre-oxidants and alternative disinfectants.

    Solution

    A complete survey of the system was conducted to evaluate water quality and other factors such as consumption rate, maintenance, economics and compliance goals. A recommendation was made to the municipality to treat the raw water with chlorine dioxide at an initial feed rate of 0.2 mg/L. This dose rate was gradually increased after eight weeks to 0.8 mg/L until a trace amount of chlorine dioxide was measured in the clear well. As the dose rate of chlorine dioxide was increased an improvement in water quality was expected allowing for a reduction in the dose rate of the primary disinfectant chlorine gas.

    Results

    Chlorine dioxide effectively lowered TTHM and HAA5 levels by 30% over the same period a year ago. TOC levels have consistently been reduced by 25% or more using the new process which includes enhanced coagulation. The applied chlorine dose rates have also been reduced from 3.4 mg/L to 1.8 mg/L during the same month in consecutive years.

     

    top of page
    Print
    Contact Us
    Get help now
    Contact

    Related Products

     Chlorine Dioxide Generation Systems

    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID