SIEMENS

 

Traveling Water Screens Upgrade Impacts Millstone Point Facility 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
      • Contact Us
      • Request A Proposal
    • Applications
      • Aquatic Water Treatment
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
    • Drinking Water Treatment
      • Arsenic Removal
      • Disinfection
      • Disinfection By-Products Removal
      • Dissolved Metals Removal
      • Fluoridation
      • Hexavalent Chrome Removal
      • Iron and Manganese Removal
      • Perchlorate Removal
      • TOC Reduction
      • VOC Removal
      • Water Clarification and Filtration

    Traveling Water Screens Upgrade Impacts Millstone Point Facility

    Challenge

    The Millstone Point Facility, operated by Northeast Utilities, identified multiple issues in their plant operation revolving around macrofouling problems due to large flow requirements and the intake structure orientation.

    1. Inadequate travel speed for storm-induced algae loads.
    2. Insufficient head capacity for storm-induced algae loads.
    3. An excess corrosion rate of TWS materials.

    Solution

    Design changes were based on testing done in Wisconsin with several hundred pounds of Long Island Sound algae that had been shipped in. This testing led the team to make the following changes and upgrades to the plant:

    • Replace the two-speed TWS capability with four-speed.
    • Increase the maximum speed from 20 feet per minute to 32 feet per minute.
    • Increase the motor horsepower from 7.5 to 20.
    • Replace carbon steel baskets with nonmetallic baskets.
    • Replace the carbon steel frame with a 3161 stainless steel frame.
    • Increase head capacity from 5 feet to 10 feet of water.
    • Add cathodic protection, a rear-side debris spray header for emergency and back flushing use, and screen wash blowback valves.

    Results

    • The new high-capacity installations have enabled the facility to stay on-line during severe storms.
    • Outage time caused by traveling water screens has been reduced by over 10 days per year. This will save $7.6 million over a ten year period.
    • Further savings will be realized from reduced corrosion-related failures of carbon steel components and the ability to clean the screenwash piping on-line.

     

    top of page
    Print
    Contact Us
    Typical Through Flow TWS
    Get help now
    Contact

    Related Products

    Through Flow Traveling Water Screen

    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID