SIEMENS

Arazona Water Supply Arsenic Removal Case Study 

GFH Media Removes Arsenic in Arizona Water Supply 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
    • Applications
      • Aquatic Water Treatment
      • Corrosion and Biofouling Protection
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
    • Drinking Water Treatment
      • Aeration and Gas Stripping
      • Arsenic Removal
      • Disinfection
      • Disinfection By-Products Removal
      • Dissolved Metals Removal
      • Fluoridation
      • Hexavalent Chrome Removal
      • Hydrogen Sulfide Removal
      • Iron and Manganese Removal
      • Mercury Removal
      • Perchlorate Removal
      • Softening - Hardness Removal
      • Taste and Odor Control
      • TOC Reduction
      • VOC Removal
      • Water Clarification and Filtration
      • Water Quality Analyzers and Process Control

    GFH Media Removes Arsenic in Arizona Water Supply

    Challenge

    Like many communities in the desert southwest, Phoenix, Arizona’s water supply includes wells with arsenic concentrations exceeding 10 ppb.  Long before the USEPA revised the arsenic rule from 50 parts per billion (ppb) to 10, the City of Phoenix began bench and pilot scale studies for arsenic removal options.  Early investigations focused on well-known processes like activated alumina and ion exchange as well as less proven concepts such as coagulation-assisted microfiltration.  Later, they added adsorption media technology to the study.

    The City considered cost as well as other factors like ease of operation, lower required operator attention and reduced waste generation.  They were leaning toward iron media adsorption as their technology of choice.

    Solution

    After carefully evaluating all of the factors, as well as bench-scale and pilot study data, the City selected a granular ferric hydroxide (GFH™) adsorption media from General Filter to treat water at its well #280 site.  Operated in a fixed-bed adsorber, the arsenic removal system uses 60,000 lbs. of ferric-based, non-regenerative media to primarily remove arsenic from Phoenix’s well site.  Other constituents are well below drinking water standards.

    The total flow for well #280 is 2.53 million gallons per day (mgd).  Only 1.5 mgd of the flow is treated, with the balance bypassing treatment and blending with the treated water.  The ratio of blending is controlled so that a maximum combined effluent of 8 ppb or less is maintained outside of the plant. 

    The GFH media is installed in two 14-ft diameter pressure vessels, allowing the existing well pumps to be used.  Piping to the contactors is arranged so that either can be the lead or lag vessel.  During operation, water is simply passed through the vessels containing the GFH media where arsenic is adsorbed.  Chemical pre-conditioning or pH adjustment is not required as part of the treatment process.  Treated water is blended in a storage tank prior to distribution to the system.
    Once the media reaches its adsorption capacity, media in the lead vessel is removed and replaced with new media.  Spent media is stored in a storage area before being TCLP-tested and hauled away to landfill.

    Results

    After a year of operation, the reported results of the arsenic removal plant are better than anticipated.  More than 35,000 bed volumes have passed through the GFH media with an effluent arsenic concentration remaining below detection.  In addition, there have been no backwash events based on headloss build-up during this time.  Operational since September 2003, the facility requires approximately eight hours per week of city staff time for routine operation and maintenance.

    top of page
    Print
    Contact Us
    GFH Media
    Get help now
    Contact

    Related Products

    GFH Arsenic Removal System

    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID