SIEMENS

 

Chertsey WTW Microfiltration Plant – Surrey, United Kingdom 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
      • Contact Us
      • Request A Proposal
    • Applications
      • Aquatic Water Treatment
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
    • Drinking Water Treatment
      • Arsenic Removal
      • Disinfection
      • Disinfection By-Products Removal
      • Dissolved Metals Removal
      • Fluoridation
      • Hexavalent Chrome Removal
      • Iron and Manganese Removal
      • Perchlorate Removal
      • TOC Reduction
      • VOC Removal
      • Water Clarification and Filtration

    Chertsey WTW Microfiltration Plant – Surrey, United Kingdom

    Challenge

    Chertsey WTW Surrey, United Kingdom MEMCOR® CS Chertsey Water Treatment Works has supplied the local population with good quality water for decades. However, due to the increased demands on the water company as a result of deterioration in source water quality and the need to alternate sources because of dwindling river flows, greater demand is being upon the treatment works

    These extra demands and in particular the strategy for cryptosporidium can be handled in a number of ways that will satisfy the Regulator. However, the Water Company needed to implement a cost effective and robust solution that satisfied their specific situation.

    Solution

    Three Valleys Water Company Limited embarked upon a series of tests to select their preferred membrane suppliers on a framework basis. These tests revealed that The MEMCOR CS membrane system provided excellent water quality in a very compact footprint, whilst offering cost competitiveness compared to more traditional methods of treatment. The MEMCOR CS is able to produce consistent treated water quality irrespective of the feed water quality whilst enabling the operators to monitor integrity assuring the complete removal of all bacteria, algae, turbidity and pathogens such as cryptosporidium.

    This fully automated plant has a high degree of flexibility built in to it enabling it to handle a range of flow rates. The submerged configuration of membranes substantially reduces the number of automatic valves required when compared to a pressurized membrane system making the plant simple in operation and maintenance.

    Black & Veatch Limited (Contracting) were selected by Three Valleys to act as main contractors for this contract.

    Results

    Raw water passes through coarse strainers and into the membrane “cell” by means of a filtrate suction pump. Six cells each containing 192 membrane modules are able to produce an output of 41 MLD. Each module consists of Polyvinylidene Difluoride membrane fibre having a nominal pore size of 0.1 micron. The filtrate suction pump delivers the water to downstream ozonation and GAC. Backwashes are carried out periodically using either sodium hypochlorite or sulphuric acid. The membranes are cleaned in-situ without the need to withdraw them to a separate tank.

    The plant design is such that maintenance can be carried out on a rack of membranes whilst the remainder of the plant continues to operate in service. Three Valleys WTW solved its big challenge to provide membrane treatment at a number of its works throughout West London and the home counties to ensure high quality potable water.

    top of page
    Print
    Contact Us
    Get help now
    Contact

    Related Products

    MEMCOR® CS Submerged Microfiltration System

    Download Case Study
    Full Case Study

    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID