SIEMENS

 

California Water Services Company Commences 10-year Contract for Treatment of Nitrate and Perchlorate in Community Water System 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
      • Contact Us
      • Request A Proposal
    • Applications
      • Aquatic Water Treatment
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
    • Groundwater Remediation
      • Arsenic Removal
      • Dissolved Metals Removal
      • Hexavalent Chrome Removal
      • Nitrate Removal
      • Organic Chemicals Removal
      • Perchlorate Removal
      • VOC Removal

    California Water Services Company Commences 10-year Contract for Treatment of Nitrate and Perchlorate in Community Water System

    Challenge

    California Water Service Company had recently acquired another water company who was responsible for this community drinking water system. The community has approximately 100 connections and is located in a remote agricultural section of the Central Valley. Annual well testing had shown levels of Nitrate at or near the Maximum Contamination Level (MCL) of 45 ppm NO3, also perchlorate was found in the groundwater at levels above the PublicHealth Goal (PHG) at 10 ppb.

    Solution

    Siemens Water Technologies provided a unique treatment system where the water is first treated for removal of perchlorate using single use ion exchange resin and then nitrate removal with a traditional regenerable ion exchange media. However, since the water purveyor could not handle on site waste streams the nitrate removal resin is regenerated off site.  The resin is sluiced in and out of the fixed tanks using a closed process that ensures the cleanliness of the media and complies with State Health Department sanitization requirements for ion exchange resins.

    Results

    The service-based solution significantly reduces the amount of manpower that the water company needs to maintain for site operation.

    The nitrate treatment system uses off-site regeneration at a Siemens Water Technologies facility that reduces overall operating costs for treatment of the nitrate and eliminates generation of any liquid or solid waste stream at the site.

    The financial arrangement for this project allowed the water company to plan their costs over a 10 year period versus the capital investment necessary to install a new treatment system.

    Download the full case study

    top of page
    Print
    Contact Us
    California Water Services, Porterville, CA PP
    Get help now
    Contact

    Related Services

    Learn more about our ion exchange service options

    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID