Iron & Manganese Removal from Groundwater 

Iron & Manganese Removal from Groundwater 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Groundwater Remediation
    • Arsenic Removal
    • Chemical Feed and Control
    • Dissolved Metals Removal
    • Hexavalent Chrome Removal
    • Iron & Manganese Removal
    • Landfill Leachate Treatment
    • Nitrate Removal
    • Organic Chemicals Removal
    • Perchlorate Removal
    • VOC Removal
  • Iron & Manganese Removal

Iron & Manganese Removal from Groundwater

Iron and manganese are undesirable in groundwater because of their effect on the appearance and taste of the water, their ability to cause staining, and the health effects of manganese.

Iron and Manganese Removal
Filtration with Greensand Media provides a one-step treatment option for Iron and Manganese Removal

Iron and manganese occur naturally in water, especially groundwater. Neither of the elements causes adverse heath effects; they are, in fact, essential to the human diet. However, water containing excessive amounts of iron and manganese can stain clothes, discolor plumbing fixtures, and sometimes add a "rusty" taste and look to the water.

The US Environmental Protection Agency and the Safe Drinking Water Act (SDWA) has established a secondary (aesthetic) standard Maximum Contaminant Level (MCL) for iron in drinking water of 0.3 parts per million (ppm); for manganese it is 0.05 ppm. At present, the US Environmental Protection Agency (EPA) has not set health standards for either iron or manganese in drinking water, therefore, stated MCLs are not enforceable. However, a health based standard for manganese is possible. Manganese may affect neurological and muscle function in humans. The Department of Environmental Services (DES) Health Risk Assessment Program has adopted an interim health based standard for manganese of 0.84 mg/L.

How iron and manganese are removed depends on the type and concentration, and this helps determine the best procedure and treatment system to use. Iron and manganese can be present in water in one of three basic forms: dissolved, particulate and colloidal. The predominance of one form over another is dependent on the water's pH. The two most common treatment methods are removal by oxidation/filtration and adsorbing onto ion exchange resins.

Oxidation involves the introduction of an oxidizing agent which chemically reacts with the iron or manganese to form an insoluble particle which can then be physically filtered out through a media bed.

Oxidation can be carried out one of the following methods:

  • aeration - blowing/spraying air through the water
  • addition of dissolved chemical oxidants - chlorine, chlorine dioxide and potassium permanganate (KMnO4)
  • adsorption - greensand media and activated carbon

The process of oxidation followed by filtration is fairly easy and is often the treatment of choice. The use of ion exchange resins for the removal of iron and manganese has limited application due to the requirement that the contaminants be in dissolved form and at very low levels. This is due to the tendency of oxygen to react with the iron and managanes and therefore, increase the potential for plugging and buildup on the resin surface. Iron fouling is a common, and sometimes, irreversible problem with ion exchange treatment.

Treatment technologies for Iron and Manganese Removal from Groundwater:

Aeration
Activated Carbon
Media Filtration
Chemical Oxidation
Ion Exchange

top of page

Contact Us

For more information about iron and manganese removal in groundwater, contact the Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Iron & Manganese Removal Case Study

Northeast Super Fund Site Uses Mobile Treatment for Groundwater Iron Removal

This client operates a groundwater treatment facility at a Super Fund site where groundwater is pumped to a VOC stripper for the removal of TCE which is then re-injected into the aquifer.  High iron levels in the groundwater caused fouling of pumps, pipes and well casings.  This fouling threatened the reliability of the process in terms of flow.

Read Full Case Study

Iron and Manganese Removal Case Study
top of page
Print
Contact Us

Featured Products and Services

AERALATER® Packaged System
ANTHRA/SAND™ Media
Forced Draft Aerator System
Ion Exchange Systems
Mobile Water Treatment Service

Iron and Manganese Removal Case Studies

Packaged Iron and Manganese Removal System Ensures Water Quality, Reduces Maintenance Costs
Procuring a Water Treatment Solution Using an Uncommon Method
Northeast Super Fund Site Uses Mobile Treatment for Groundwater Iron Removal
Mobile Treatment Provides Well Water Treatment for Temporary Drinking Water Supply at Construction Site

Product Documentation

Iron and Manganese Removal Brochure

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID