Landfill Leachate Treatment 

Landfill Leachate Treatment 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Groundwater Remediation
    • Arsenic Removal
    • Chemical Feed and Control
    • Dissolved Metals Removal
    • Hexavalent Chrome Removal
    • Iron & Manganese Removal
    • Landfill Leachate Treatment
    • Nitrate Removal
    • Organic Chemicals Removal
    • Perchlorate Removal
    • VOC Removal
    • carbon-treat-contaminated-wells
    • pv-varbon-rainwater-runoff
  • Landfill Leachate Treatment

Landfill Leachate Treatment

Landfill leachate is generated from liquids existing in the waste as it enters a landfill or from rainwater that passes through the waste within the facility. The leachate consists of different organic and inorganic compounds that may be either dissolved or suspended. An important part of maintaining a landfill is managing the leachate through proper treatment methods designed to prevent pollution into surrounding ground and surface waters.

PACT Integrated Systems
PACT Integrated Systems for landfill leachate treatment

If leachates have a distinguishing characteristic, it is that they are variable.  Flows change based on the weather  – increasing during rainy periods, decreasing during dry and waste concentrations can change dramatically over the life of the landfill.   As a result, no landfill leachate is constant over time, and no two leachates are the same.

Leachate can consist of many different organic and inorganic compounds that are typically either dissolved or suspended in the wastewater.  High concentrations of chemical oxygen demand (COD)associated, BOD, nitrogen, phenols, pesticides, solvents and heavy metals are common in these systems.

Leachate treatment technologies fall into two basic types, biological and physical/chemical. In larger systems and depending on the treatment goals, integrated systems which combine the two are often used.

The most common biological treatment is activated sludge, which is a suspended-growth process that uses aerobic microorganisms to biodegrade organic contaminants in leachate. With conventional activated sludge treatment, the leachate is aerated in an open tank with diffusers or mechanical aerators.

Siemens Water Technologies' PACT® systems combine biological treatment (activated sludge) with adsorption (powdered activated carbon) so that physical and biological treatment occur simultaneously. The system removes biodegradable and non-biodegradable pollutants in a single process. The single-step treatment process results in significant cost and performance advantages over individual systems such as activated sludge and granular carbon.  We can also provide inclined plate separators or ion exchange systems for metals removal, if necessary, as well as rapid sand filters for suspended solids control and bulk chemical handling equipment.

Landfill leachate has also been effectively treated by the rotating biological contactor (RBC) process.  The RBC is a biological process consisting of a large disc with radial and concentric passages slowly rotating in a concrete tank. During the rotation, about 40 percent of the media surface area is in the wastewater. The rotation and subsequent exposure to oxygen allows organisms to multiply and form a thin layer of biomass. This large, active population causes the biological degradation of organic pollutants. Excess biomass shears off at a steady rate and is then carried through the RBC system for removal in a clarifier.

Activated carbon adsorption systems have also been used in the treatment of landfill leachates for removal of dissolved organics, however, they are generally considered one of the more expensive treatment options and often, must be combined with other treatment techologies to achieve desired results.

Landfill Leachate Treatment Technologies:

Biological Treatment - Integrated/Advanced WW Treatment
Biological Treatment - Mechanical Aeration WW Treatment
Activated Carbon Adsorption

top of page

Contact Us

For more information about landfill leachate treatment, contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Landfill Leachate Treatment Case Study

PACT® System Successful on Landfill Leachate, Groundwater in Florida

The Zemel Road Municipal Solid Waste Landfill serving Charlotte County, FL, had to meet new state standards for deepwell injection of treated leachate and groundwater. Located in Punta Gorda, the landfill receives solid waste from throughout the county of about 125,000 population. Bentonite slurry walls direct the leachate into a French drain type collection system, then it is pumped to an on-site treatment plant.

To meet the new standards, the landfill needed a technology that could handle varying concentrations of contaminants, while fitting easily onto the site. Design contaminant levels were 1,000 milligrams per liter COD, 500 mg/l BOD, and 500 mg/l suspended solids.

Read Full Case Study

Landfill Leachate Case Study
top of page
Print
Contact Us

Featured Products and Service

Rotating Biological Contactor Systems
PACT® Integrated Treatment Systems
Activated Carbon Systems
Powdered Activated Carbon Media
Wastewater Ion Exchange Service
Hazardous/Non-hazardous Waste Treatment and Recycling Service

Landfill Leachate Treatment Case Studies

PACT® System Successful on Landfill Leachate, Groundwater in Florida
Landfill Leachate System at South Central Counties Solid Waste Agency Treats 12,000 Gallons Per Day of Leachate
PACT® System Provides Leachate Management at Citrus County, Florida

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID