Groundwater Dissolved Metals Removal 

Groundwater Dissolved Metals Removal 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Groundwater Remediation
    • Arsenic Removal
    • Chemical Feed and Control
    • Dissolved Metals Removal
    • Hexavalent Chrome Removal
    • Iron & Manganese Removal
    • Landfill Leachate Treatment
    • Nitrate Removal
    • Organic Chemicals Removal
    • Perchlorate Removal
    • VOC Removal
    • carbon-treat-contaminated-wells
    • pv-varbon-rainwater-runoff
  • Dissolved Metals Removal

Dissolved Metals Removal from Groundwater

Many dissolved metals have been found in harmful concentrations in groundwaters destined for both potable drinking water and non-potable use.  The presence of dissolved metals can be naturally occurring contamination as well as being introduced from industrial pollution.  Dissolved metals in groundwater sources causes concerns from the viewpoint of human consumption, as well as for industries using it for influent process, recycle and reuse purposes.

Removable Service Ion Exchange Vessels
Removable Service Ion Exchange Vessels

Urbanization and water demand in areas of industrial activity has increased the frequency of problem metals in groundwater sources used for both drinking (potable) needs as well as industrial (non-potable) processes.  

Groundwater used for drinking water applications is typically found in aquifers and wells.  In these cases, some small quantities of certain heavy metals are actually acceptable because they are nutritionally essential for a healthy life, but large amounts of them may cause acute or chronic toxicity (poisoning). Trace elements such as iron, copper, manganese, and zinc are commonly found naturally in foods we consume or as part of a vitamin supplement.  

The metals most often linked to human poisoning have links to learning disabilities; cancers and death are typically copper, nickel, cadmium, chrome, arsenic, lead and mercury.  Many of these metals are required by humans in trace amounts but in larger, persistent dosages, these heavy metals become toxic when they are not metabolized by the body and accumulate in the soft tissues. Heavy metal toxicity can result in damaged or reduced mental and central nervous function, lower energy levels, and damage to blood composition, lungs, kidneys, liver, and other vital organs.

The most commonly encountered toxic heavy metals include:

  • Arsenic
  • Lead
  • Mercury
  • Cadmium
  • Iron
  • Aluminum

Other heavy metals of concern include:

  • Antimony
  • Chromium/chrome
  • Cobalt
  • Copper
  • Manganese
  • Nickel
  • Uranium
  • Vanadium
  • Zinc

Groundwater used for non-potable applications, such as feed to an industrial and/or manufacturing process, also requires attention and removal of dissolved metals.  In addition to the concerns already stated for human health and the environment, metal removal occurs in industrial applications in order to meet influent water quality requirement needed by the manufacturing process and equipment. 

Siemens can offer a wide range of treatment technologies depending on the specific contaminant to be reduced.

Ion exchange is a proven technology with effective treatment results for the removal of dissolved metals.  Siemens Water Technologies offers permanent, hard-piped ion exchange treatment systems and removal system, each containing contaminant-specific treatment resins.  Alternatively, activated carbon has also proven effective for adsorption of certain metals from contaminanted sources.

Siemens Water Technologies offers a service-based treatment option for handling dissolved metals contamination. For non-potable applications, our Wastewater Ion Exchange (WWIX) approach integrates equipment and service option combinations, thereby minimizing a plant’s capital investment and reduces overall space requirements.  The system vessels are selected based upon available manpower, space limitations, access limitation and the specific water quality required.  Based on the particulars of the contaminant to be removed and inlet quality requirements, we have access to a variety of ion exchange resins and other removal medias, such as activated carbon.  Wastewater Ion Exchange provides the ultimate flexibility to add or remove treatment capacity as your business grows or compliance limits change.  If needs change, we can simply change the media types and/or tank size, thereby saving our customers significant capital expense.

Once exhausted, the exchange vessels are removed and replaced with fresh, DOT-compliant vessels and returned to service. For non-potable applications, exhausted vessels are transferred to our central treatment and processing facility where the hazardous/non-hazardous contaminants are removed from the media/resin for reuse. 

For waters destined for potable use and drinking water applications, Siemens offers Potable Ion Exchange (PIX) Service.  PIX utilizes potable ion exchange resin canisters for the removal of organic and inorganic contaminants in surface and groundwater sources to meet drinking water standards. Each application is examined to determine the system configuration that best meets current and future needs.  Once the treatment media is spent, or reaches the end of it's useful life, the potable canisters are removed from the site and delivered to a local regeneration facility for destruction and/or landfill.

Both WWIX and PIX minimize the need for handling and on-site storage of chemicals and wastes for improved safety and compliance at your site. This option also saves valuable manufacturing space while minimizing your maintenance and installation requirements.
 

Dissolved Metals Removal Technologies for Your Groundwater Remediation  Applications

Ion Exchange
Activated Carbon Adsorption

top of page

Contact Us

For more information about dissolved metals removal in groundwater treatment, contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Groundwater Dissolved Metals Removal Case Study

Hexavalent Chrome Contamination Treatment For Reinjection

In March 2003, Siemens Water Technologies, formerly USFilter, was awarded a contract to provide design, installation, training, and off site recovery for a chromium contaminated groundwater supply in Texas. The site is the location for a number of chrome plating shops that have since gone out of business. The project is now part of an EPA superfund cleanup.

Read Full Case Study

Metals Removal Case Study
top of page
Print
Contact Us

Featured Products and Services

Demineralizer/Deionizer Systems
Replacement Ion Exchange Resins
Activated Carbon Medias
Activated Carbon Filtration Systems
Wastewater Ion Exchange (WWIX) Service
Potable Ion Exchange (PIX) Service
Hazardous/Non-Hazardous Waste Treatment and Recovery

Groundwater Dissolved Metals Removal Case Studies

Ion Exchange Treatment of Regulated Metals in Coal Ash Found to be Efficient in Power Industry
School District Seeks EPA Arsenic Removal Compliance and Permitting
American Gypsum Purchases Arsenic Removal System to Treat the Company's On-Site Well and Meet New Regulations
Siemens Delivers Temporary Arsenic Treatment System While Permanent Solution is Engineered for Bucks County Water Authority
Cyanide Contamination at Manufactured Gas Plant Treated With Wastewater Ion Exchange Service
Historic Mine Uses Wastewater Ion Exchange Service for Copper and Cobalt Removal

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID