Organic Chemicals Removal from Groundwater 

Organic Chemicals Removal from Groundwater 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Groundwater Remediation
    • Arsenic Removal
    • Chemical Feed and Control
    • Dissolved Metals Removal
    • Hexavalent Chrome Removal
    • Iron & Manganese Removal
    • Landfill Leachate Treatment
    • Nitrate Removal
    • Organic Chemicals Removal
    • Perchlorate Removal
    • VOC Removal
    • carbon-treat-contaminated-wells
    • pv-varbon-rainwater-runoff
  • Organic Chemicals Removal

Organic Chemicals Removal from Groundwater

As surface waters continue to be threatened by industrial pollution, groundwaters are increasingly being looked to as sources for both potable, drinking water and other non-potable applications.  Treatment of such waters for the removal of organic contaminants varies based on the intended uses, however, in most cases, even trace amounts of the contaminants require some level of removal to meet drinking water and/or makeup water requirements.

Organic Chemicals Removal
Activated carbon is designated as best available technology for organic chemical removal

Organic substances are composed of two basic elements, carbon and hydrogen, and are often responsible for taste, odor, and color problems in groundwaters.  As such, treatment is used generally to improve aesthetically objectional water.

Sources of organic compounds (VOC’s, taste & odor compounds, disinfection byproducts, and free chlorine) found in groundwaters may include leaking underground gasoline/storage tanks, agricultural runoff containing herbicides or pesticides, solid waste or hazardous waste landfills, and improperly disposed industrial/chemical waste.

The ability of organic compounds to cause health effects varies greatly from those that are highly toxic, to those with no known health effect. The extent and nature of the health effect will depend on many factors including level of exposure and length of time exposed. Eye and respiratory tract irritation, headaches, dizziness, visual disorders, and memory impairment are among the immediate symptoms that some people have experienced soon after exposure to some organics.

The technologies most suitable for organic contaminant removal in process waters are granular activated carbon (GAC) and aeration. 

GAC has been designated by the U.S. Environmental Protection Agency (EPA) as the best available technology (BAT) for organic chemical removal.  Activated carbon adsorption provides an effective and reliable treatment for removing organic contaminants and is suitable for treating a wide range of organics over a broad range of concentrations.  GAC filtration will also remove chlorine.

GAC filtration is recognized by the Water Quality Association as an acceptable method to maintain certain drinking water contaminants within the limits of the EPA National Drinking Water Standards.  Organics that are readily adsorbed by activated carbon include:  

  • Aromatic solvents (benzene, toluene, nitrobenzenes)
  • Chlorinated aromatics (PCBs, chlorobenzenes, chloroaphthalene)
  • Phenol and chlorophenols
  • Polynuclear aromatics (acenaphthene, benzopyrenes)
  • Pesticides and herbicides (DDT, aldrin, chlordane, heptachlor)
  • Chlorinated aliphatics (carbon tetrachloride, chloroalkyl ethers)
  • High molecular weight hydrocarbons (dyes, gasoline, amines, humics)  

Various types of GAC are available for removing organics from water, however, the most frequently used carbon in the US. is coal-based carbon due to its hardness, adsorption capacity, and ease of availability. 

Siemens Water Technologies offers a wide range of activated carbon medias, adsorber systems and support services.  We feature Westates® activated carbon medias which are extensively quality checked at our State of California certified environmental and carbon testing laboratory. Siemens’ laboratory is fully equipped to provide complete quality control analyses using ASTM standard test methods in order to assure the consistent quality of all Westates® activated carbons.

Additionally, Siemens offers reactivated carbon services.  Carbon reactivated ends the responsibility of "chain of custody" of the waste producer and is considered a "green alternative" to traditional landfilling of spent carbons.  The reactivation process recycles spent carbons into new activated carbon materials that continue to provide excellent performance for many treatment applications.  Siemens Water Technologies has over 20 years of experience in carbon reactivation and operates three reactivation facilities in the US serving  both the East and West coasts for reactivation of spent carbon. 

Treatment Technologies for the Removal of Organic Chemicals from Groundwater

Aeration
Activated Carbon Adsorption

top of page

Contact Us

For more information about organic chemicals removal in groundwater, contact the Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Organic Chemicals Removal from Groundwater Case Study

Removal of Nitrates and TCP Make San Jerardo, CA Drinking Water Safe for Residents

In March 2006, members of the San Jerardo, CA community reported skin rashes from water use.  Upon testing the water, nitrates and trichloropropane (TCP) were both found to be at levels well above the regulatory limit.  High levels of nitrates are common in many wells, and it is believed that the surrounding agricultural area led to the TCP contamination.  Drinking water regulations require nitrate to be less than 45 ppm and TCP less than 5 ppt. At the time of testing, the nitrate level was at 78 ppm and TCP was at 80 ppt.

Read Full Case Study

Organic Chemicals Removal Equipment
top of page
Print
Contact Us

Featured Products and Services for Organic Chemicals Removal

Liquid Phase Activated Carbons
Liquid Phase Carbon Adsorber Equipment
Carbon Exchange Service
Carbon Reactivation Service
Aerator Systems

Organic Chemicals Removal from Groundwater Case Studies

Carbon Adsorber System Helps Fertilizer Manufacturer Treat Organics in Rainwater Runoff
Siemens Provides Activated Carbon for Treatment of Contaminated Wells in Drought-Ridden State
Removal of Nitrates and TCP Make San Jerardo, CA Drinking Water Safe for Residents
Cyanide Contamination at Manufactured Gas Plant Treated With Wastewater Ion Exchange Service

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID