Perchlorate Removal from Groundwater 

Perchlorate Removal from Groundwater 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Groundwater Remediation
    • Arsenic Removal
    • Chemical Feed and Control
    • Dissolved Metals Removal
    • Hexavalent Chrome Removal
    • Iron & Manganese Removal
    • Landfill Leachate Treatment
    • Nitrate Removal
    • Organic Chemicals Removal
    • Perchlorate Removal
    • VOC Removal
    • carbon-treat-contaminated-wells
    • pv-varbon-rainwater-runoff
  • Perchlorate Removal

Perchlorate Removal from Groundwater

Perchlorate salts, such as ammonium perchlorate and potassium perchlorate, are man-made compounds used as combustion accelerants, primarily in solid-fueled rockets and missiles.  It can also be found in some munitions, fireworks, road flares and is even thought to exist naturally in some nitrate-based fertilizer products.  Perchlorate exposure has been linked to hormonal balances and impedes human reproduction and development.

Perchlorate Removal System
Ion Exchange Resin System for Perchlorate Removal

Manufacturing waste and improper disposal of perchlorate-containing compounds are increasingly being found in groundwater and local drinking water wells where these conditions exist.

The US Environmental Protection Agency, federal agencies and local governments are currently assessing the potential human health risks posed by perchlorate exposure. Currently, there are no enforceable perchlorate stafety standards, however, a few US states have adopted perchlorate actionable levels, among them CA and MA.  Perchlorate is one of a newly recognized group of toxins called endocrine disrupters, which can alter hormonal balances and impede human reproduction and development.  

The EPA’s protective health level for perchlorate in drinking water is a dose estimate of less than 1 part per billion (ppb). Many  perchlorate plumes in the United States, including the Colorado River, are believed to be in the range between four and 100 ppb.  It is estimated that perchlorate contamination occurs in groundwater, drinking water sources in at least 22 US states and has been found in many nutritionally important foods such as milk, lettuce and other leafy green vegetables.

Ion exchange is the most frequently used treatment technology for perchlorate removal.  This technology removes the perchlorate ions from the aqueous phase by replacing them with the anion present in the ion exchange resin.  As contaminated water is passed through the resin, contaminant ions are exchanged for other ions such as chlorides or hydroxides in the resin. 

Siemens Water Technologies offers both permanent, hard-piped and removable ion exchange treatment system options.  With permanent systems, ion exchange resins must be periodically regenerated to remove the adsorbed contaminants and replenish the exchanged ions.  Regeneration water and spent resin containing high levels of perchlorate would require additional treatment prior to disposal or reuse.

Siemens also offers a service-based treatment option for handling perchlorate contamination. For non-potable applications, our Wastewater Ion Exchange (WWIX) approach integrates equipment and service option combinations, thereby minimizing a plant’s capital investment and reduces overall space requirements.  The system vessels are selected based upon available manpower, space limitations, access limitation and the specific water quality required.  Based on the particulars of the contaminant to be removed and inlet quality requirements, we have access to a variety of ion exchange resins and other removal medias.  Wastewater Ion Exchange provides the ultimate flexibility to add or remove treatment capacity as your business grows or compliance limits change.  If needs change, we can simply change the media types and/or tank size, thereby saving our customers significant capital expense.

Once exhausted, the exchange vessels are removed and replaced with fresh, DOT-compliant vessels and returned to service. For non-potable applications, exhausted vessels are transferred to our central treatment and processing facility where the hazardous/non-hazardous contaminants are removed from the media/resin for reuse. 

For waters destined for potable use and drinking water applications, Siemens offers Potable Ion Exchange (PIX) Service.  PIX utilizes potable ion exchange resin canisters for the removal of organic and inorganic contaminants in surface and groundwater sources to meet drinking water standards. Each application is examined to determine the system configuration that best meets current and future needs.  Once the treatment media is spent, or reaches the end of it's useful life, the potable canisters are removed from the site and delivered to a local regeneration facility for destruction and/or landfill.

Both WWIX and PIX minimize the need for handling and on-site storage of chemicals and wastes for improved safety and compliance at your site. This option also saves valuable manufacturing space while minimizing your maintenance and installation requirements.

In both cases, single-use, non-regenerable ion exchange resins may alternativelhy be used.  These resins are removed when spent and thermally destroyed, thereby eliminating disposal liabilities of both the waste and wastewaters containing perchlorate.  

Ion exchange is often preceded by treatments such as filtration and oil-water separation to remove organics, suspended solids, and other contaminants that can foul the resins and reduce their effectiveness.  


Perchlorate Removal Technologies for Your Groundwater Remediation Applications

Ion Exchange Systems
Granular Activated Carbon (GAC) Systems
Reverse Osmosis (RO) Systems

top of page

Contact Us

To learn more about perchlorate removal, please contact the Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com

top of page

Perchlorate Removal from Groundwater Case Study

Aerospace Manufacturer Utilizes Service Ion Exchange to Solve Perchlorate Contamination

Siemens Water Technologies worked with an east coast aerospace manufacturer to provide a solution to the perchlorate contamination affecting their facility's drinking water supply for on-site personnel.  In response to new drinking water standards being established by the EPA, the customer sought a system which would treat the contamination and bring the perchlorate levels below its detection limit of 4 ppb.

Read Full Case Study

Perchlorate Removal Case Study
top of page
Print
Contact Us

Featured Products and Services for Perchlorate Removal from Groundwater

Replacement Ion Exchange Resins
Demineralizer/Deionizer Systems
Wastwater Ion Exchange (WWIX) Service
Potable Ion Exchange (PIX) Service 
Hazardous/Non-Hazardous Waste Treatment and Recovery

Perchlorate Removal Case Studies

Ion Exchange Resin Removes Perchlorate From 2000 gpm Drinking Water Supply in California
California Water Services Company Commences 10-Year Contract for Treatment of Nitrate and Perchlorate in Community Water System
MA Condominium Complex Becomes First Recognized Perchlorate Cleanup in the State
West Coast Aerospace Manufacturer Signs Agreement to Treat Perchlorate Contamination
California Community Chooses Siemens Water Technologies for Removal of Perchlorate From Primary Drinking Wells
One of the First Full-Scale Perchlorate Treatment Systems in a Northeast US Public Drinking Water Supply Installed by Siemens
Aerospace Manufacturer Utilizes Service Ion Exchange to Solve Perchlorate Contamination

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID