Volatile Organic Compounds (VOC) Removal from Groundwater 

Volatile Organic Compounds (VOC) Removal from Groundwater 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Groundwater Remediation
    • Arsenic Removal
    • Chemical Feed and Control
    • Dissolved Metals Removal
    • Hexavalent Chrome Removal
    • Iron & Manganese Removal
    • Landfill Leachate Treatment
    • Nitrate Removal
    • Organic Chemicals Removal
    • Perchlorate Removal
    • VOC Removal
    • carbon-treat-contaminated-wells
    • pv-varbon-rainwater-runoff
  • VOC Removal

Volatile Organic Compounds (VOC) Removal from Groundwater

Volatile organic compounds (VOCs) are carbon-based chemicals that easily evaporate into gaseous forms at room temperature. Commonly referred to as solvents, the human health risks associated with exposure to VOCs vary from mild to severe and are dependent upon several factors including length of time and level of exposure.

Carbon Adsorbers for Vapor Phase VOC Control
Vapor phase carbon adsorbers available in permanent and non-hardpiped systems

Federal, state, and local regulations often limit the quantity of volatile organic compounds (VOCs) that are emitted from a variety of sources, including industrial facilities, groundwater remediation sites (air stripper or soil vapor extraction off-gas), and landfills.  Examples of compounds that have to be removed include benzene, halogenated solvents (TCE, vinyl chloride), and siloxanes.  Treatment of these various vapor sources to reduce the VOC emissions is often required to comply with regulations.

While some VOCs cause no known health effects, others are known to be highly toxic. Their effects vary and are dependent upon several factors including most notably, length of time and level of exposure.  Common symptoms associated with exposure to VOCs include eye, nose and throat irration,  nausea/vomiting, allergic skin irritation, dizziness and visual disorders.  Extended exposure in the long-term can result in more serious conditions such as cancer, damage to the liver, kidney and central nervous system and loss of coordination.

Numerous technologies exist to perform VOC reduction in vapor streams; one of the most common methods is through the employment of granular activated carbon (GAC) in fixed bed adsorber vessels.  Many VOCs readily adsorb onto GAC, and the spent GAC can often be sent for thermal reactivation as an effective, environmentally friendly means of disposal.  

VOC Control Technologies for Your Odor and Vapor Control Applications

Activated Carbon Adsorption

top of page

Contact Us

For more information about VOC Removal,contact the Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

VOC Removal from Groundwater Case Study

Delaware Community Solves VOC Contamination in Drinking Water Supply with Activated Carbon

In the Fall of 2005, water analysis for the Town of Millsboro, DE indicated that they were exceeding the Maximum Contaminant Level (MCL) for the volatile organic compound, Trichloroethylene (TCE).  TCE has been identified by the EPA as a carcinogen.  The town's supply averaged between 70 to 90 parts per million (ppm) of trichloroethylene, which is about 14 times higher than the federal limit of 5 ppb.

Read Full Case Study

VOC Case Study
top of page
Print
Contact Us

Featured Products and Services for VOC Removal

Vapor Phase Activated Carbons   

Vapor Phase Adsorption Systems

Carbon Exchange Services

Reactivation Services

Featured Case Studies

Former Manufactured Gas Plant (MGP) Chooses Siemens and Activated Carbon System for VOC Removal
Town of Millsboro, Delaware Choose Activated Carbon Response for Emergency VOC Removal

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID