Liquid Phase Odor Control 

Liquid Phase Odor Control 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Odor and Vapor Control
    • Corrosion Control
    • Emergency Vapor Scrubbing
    • Liquid Phase Odor Control
    • Vapor Phase Odor Control
    • VOC Removal
    • Fruit Packager Utilizes Catalytic Carbon to Reduce Hydrogen Sulfide in Wastewater
    • ZABOCS BTF System Controls Odors at Florida Wastewater Treatment Plant
    • LO/PRO® Odour Control System - Knostrop, Yorkshire Water, England
  • Liquid Phase Odor Control

Liquid Phase Odor Control

The human nose is extremely sensitive to the presence of hydrogen sulfide (H2S) and detects it "as the smell of rotten eggs" in concentrations as low as 0.0001 parts per million (ppm).  Typically wastewater-related problem odor compounds are generated in the liquid phase, during the process of conveying the wastewater from its inception to treatment area.

Liquid Phase Odor Control
Liquid phase odor control

In the modern world of wastewater treatment, control of odors has moved from an afterthought to a primary design consideration for most collection and treatment facilities. As communities and other development increases in the areas surrounding these facilities, the need to address and control these nuisance odors becomes more important.

Most wastewater-related odor problems are generated via bacterial activity within the waste streams (typically referred to as liquid-phase odor). Inherently odor-causing compounds are volatile and therefore are readily released to the air when given the opportunity, at which point they are referred to as vapor-phase odor. Odor problems can therefore be effectively controlled in either phase, however, there are often practical or economic reasons to focus on a particular phase, or in an increasing number of cases, both.

Typically wastewater-related problem odor compounds are generated in the liquid phase, during the process of conveying the wastewater from its inception to treatment area. While traveling through sewer lines, the wastewater can become anaerobic or septic (the dissolved oxygen can become depleted) as a result of the metabolic processes of microbes commonly found in wastewater. 

Under anaerobic conditions, specific sulfate-reducing bacteria thrive. These microbes generate hydrogen sulfide (H2S) as a byproduct of their respiration. H2S has a low solubility in wastewater and when it escapes from the wastewater and moves into the air it is easily recognized by its characteristic offensive, rotten-egg odor. H2S can also be responsible for severe corrosion problems and toxic conditions within wastewater conveyance and treatment facilities.

Corrosion is caused due to the acidic nature of hydrogen sulfide. In underground sewers or other wastewater collection systems where visual inspection is not easily accessible, the development and concentration of hydrogen sulfide causes offensive odors and corrosion can often go undetected until significant damage or failure occurs. 

Odor-causing wastewater is typically treated by altering the biological conditions in the wastewater or by adding chemicals to either control the formation of odor-causing compounds, or react with those compounds once they are formed. Liquid-phase treatment technology is most commonly applied in wastewater collection systems or during sludge storage/processing in the wastewater. However, liquid-phase treatment is often applied in a wastewater system for downstream control at the headworks of a treatment plant. Biosolids-handling facilities also have liquid-phase odor-control challenges that can be handled in a manner similar to the methods used for wastewater.

Among the liquid-phase treatments available, Siemens Water Technologies offers the patented products, Bioxide® and Aquit® solutions, proven treatment options that do not involve the handling of chemicals/materials classified as hazardous. Used individually or in combination, these liquid-phase odor control products promote the growth of favorable biology within the wastewater and have proven highly effective in eliminating the odors before release to the atmosphere.

Other options commonly used for liquid-phase odor control include the addition of oxidizing agents such as hydrogen peroxide and chlorine-based products, sodium or calcium hydroxides and precipitants such as iron salts. While effective, the handling issues of these hazardous agents have to be taken into consideration in the selection equation.

Treatment Technologies for Liquid Phase Odor Control
Liquid Phase Odor Control

top of page

Contact Us

For more information about liquid phase odor control, contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Liquid Phase Odor Control Case Study

VX 456® Controls Odors In Sludge Dewatering Operation and Lowers Costs

An eastern U.S. municipality was using two centrifuges for dewatering 80 to 100,000 gallons-per-day of product from the sludge thickeners.  They had routinely treated the sludge for odor control by adding approximately 100 pounds per day (126 mg/L) of potassium permanganate (KMnO4) prior to the two centrifuges.  Dosage of potassium permanganate was based on the presence of hydrogen sulfide (H2S) in the liquid phase from the centrifuges.  Sulfide levels of 0.1 mg/L were common while using this treatment protocol.  The customer was concerned with the cost of the program and continued to look for alternative chemical treatment solutions to control the odor.

Read Full Case Study

Chemfeed Storage System
top of page
Print
Contact Us

Featured Products and Services for Liquid Phase Odor Control

Bioxide® Solution
Aquit® Solution
VX 456® Mixed Oxidant Solution
VersaDose™ Automated Chemical Dosing Controller

Liquid Phase Odor Control Case Studies

VX 456® Controls Odors and Reduces Costs Compared to KMnO4  Treatment Program
Successful Implementation of an Odor Control Program on a Large Scale
VX 456® Controls Odors In Sludge Dewatering Operation and Lowers Costs
Odor Control Technology Helps Las Vegas Be A Good Neighbor
Los Angeles Looks to Next Generation of Odor Control Equipment
Odor Control Technology As Part Of California Plant Expansion
Packaged Chlorine Scrubber System Provides Safe Chlorination at Remote Wells in Southern California
Singapore Odor Control Plant Ready to Go On-Line

Featured Articles

Odour Control in the Kingdom, featured in Middle East Utilities Magazine

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID