SIEMENS

 

MEMCOR® Continuous Microfiltration System Maximizes 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
    • Applications
      • Aquatic Water Treatment
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
    • Wastewater Treatment
      • Hexavalent Chrome Removal

    MEMCOR® Continuous Microfiltration System Maximizes Water Resources for the City of Scottsdale, Arizona

    Challenge

    The desert community of Scottsdale, Arizona had no natural surface water sources and a decreasing groundwater supply. Scottsdale had historically treated and disposed of its wastewater. As the city has grown, disposal of wastewater presented several problems, such as:

    • The city was paying money to give away reclaimed water – a commodity
    • The sewerage system would need upgrading, at a similar cost to the Water Campus
    • Water lost from the city would have to be replaced, at a further treatment cost

    In 1980, the State of Arizona passed the Groundwater Management Act (GMA), whereby facilities are given withdrawal credits when recharging groundwater – an attractive alternative for Scottsdale, as groundwater requires only disinfection for potable use. The Scottsdale Water Campus was developed as a water resources management facility.

    Solution

    Siemens Water Technologies supplied a MEMCOR® CMF (Continuous Microfiltration) system as a pretreatment to RO. This system consists of 24 units containing 90 modules each, with a capacity of 18.5 MGD.   

    
    

    The Water Campus contains a 50 MGD water treatment plant, a 12 MGD water reclamation plant, and an advanced water treatment facility, which consists of CMF, RO and recharge systems.

    The CMF units are designed to achieve a minimum 14-day cleaning frequency. They were also designed to run at a flux of 17.9 GFD, treating Colorado River water, and a 24.3 GFD when treating effluent.

    Results

    Since commissioning, the CMF units have consistently exceeded their performance target of a 14-day cleaning frequency.

    • CMF units on Colorado River water run at effluent flux, and when running on effluent, have been cleaning at least monthly.
    • All CMF units are operating with a Pressure Decay Test of less than 0.2 psi/min.
    • Operating costs are approximately half of the pilot trial estimated costs.
    • The CMF plant does not require a full-time operator.

    Black & Veatch won the 2001 Grand Prize Award for its design. 

    The CMF has greatly enhanced Scottsdale’s ability to meet its growing demand for water and secure future supplies.

    top of page
    Print
    Contact Us
     Scottsdale Water Campus - Arizona
    Get help now
    Contact

    Related Products

    Classic MEMCOR® CMF - Large Range Municipal Drinking Water Membrane Systems.

    Download Case Study
    Full Case Study

    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID