Wastewater Treatment Applications 

Wastewater Treatment Applications 

Water Technologies
    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Food and Beverage Industry
      • Life Sciences Industry
      • Marine Industry
      • Mining Industry
      • Oil and Gas Industry
      • Power Industry
      • Semiconductor and Solar Industry
      • Drinking Water Treatment
      • Municipal Wastewater Treatment
      • Aquatics and Leisure
      • Applications
      • About Us
      • Videos
      • Site Map
    • Applications
      • Aquatic Water Treatment
      • Corrosion and Biofouling Protection
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
      • Find a Case Study
    • Wastewater Treatment
    Alkaline Cleaner Recovery
    Archimedes / Screw Pumping
    Biological Treatment
    BOD & COD Reduction
    Chemical Feed and Control
    Clarification and Sedimentation
    Disinfection
    Dissolved Metals Removal
    Hazardous Waste Treatment
    Hexavalent Chrome Removal
    Nutrient Removal
    Oil and Water Separation
    Primary Treatment
    Secondary Treatment
    Spent Caustic Treatment
    Tertiary Treatment
    TOC Reduction
    Water Quality Analyzers and Process Control

    Sign up for our FREE newsletter.
    First Name:
    Email:
    We respect your privacy and will never sell or rent our subscriber list.
     

    Wastewater Treatment Applications

    Alkaline Cleaner Recovery

    Alkaline Cleaner Recovery

    Alkaline cleaning is performed on metal parts at different times during the manufacturing process to remove oils, coolants and other metalworking fluids prior to electroplating.

     
    Archimedes / Screw Pumping

    Archimedes / Screw Pumping

    Originally applied for drainage and irrigation, today Archimedes screws / screw pumps are commonly used in sewage treatment plants because they cope well with varying rates of flow and suspended solids.

     
     
    Biological Wastewater Treatment System

    Biological Wastewater Treatment System

    Biological wastewater treatment uses microorganisms to break down complex materials present in the wastewater. It can aid with BOD reduction, odor control and more.

     
    BOD & COD Reduction

    BOD & COD Reduction

    Having a safe BOD level in wastewater is essential to producing quality effluent. If the BOD level is too high then the water could be at risk for further contamination, interfering with the treatment process and affecting the end product.

     
     

    Chemical Feed and Control

    Chemical feed and control systems are a vital component in all wastewater treatment applications. Each chemical has its own unique set of challenges that must be taken into consideration in the design, selection and application of the feed system.

     
    Wastewater Clarification and Sedimentation

    Clarification and Sedimentation

    Wastewater Clarification, or sedimentation, is a common and essential process in municipal and industrial wastewater treatment plants.

     
     
    Wastewater Disinfection

    Disinfection

    Wastewater disinfection systems prevent the growth of microorganisms, or pathogens, that produce human diseases. Careful measures must be taken when trying to do away with these microorganisms.

     
    Dissolved Metals Removal from Wastewater

    Dissolved Metals Removal

    Industrial wastewaters containing dissolved metals are treated to reduce the metal contaminants to meet discharge requirements and/or achieve the water quality level needed for reuse and recycling.

     
     
    Hazardous Waste Treatment

    Hazardous Waste Treatment

    Hazardous wastes are generated as the result of treatment steps performed on industrial wastewaters prior to discharge, or contaminant-containing groundwaters. The treatment process produces a residual waste, including sludge and spent media.

     
    Hexavalent Chrome Removal from Wastewater

    Hexavalent Chrome Removal

    The US EPA has established standards that require the destruction of chromates prior to discharge to avoid the potential risks of surface and drinking water contamination.

     
     
    technologies for Industrial wastewater pretreatment

    Industrial Wastewater Pretreatment

    Industrial wastewater pretreatment is the first step in wastewater treatment. Many industries use water directly or indirectly and produce a wet waste. Water sources can be different and impurities in the water will differ also.

     
    Nutrient Removal

    Nutrient Removal

    Nutrient removal is achieved by reducing the levels of nitrogen and phosphorus levels with advanced wastewater technologies. Higher quality wastewater effluent is the result of this process.

     
     
    Oil/Water Separation

    Oil Water Separation

    Wastewater oil water separation is a process that many refineries or other oil processors undergo. Siemens provides applications that can successfully separate oil from wastewater.

     
    Primary Wastewater Treatment

    Primary Wastewater Treatment

    Primary wastewater treatment, the second step in the wastewater treatment process, involves the physical separation of suspended solids from the wastewater flow using gravity filters.

     
     
    Secondary Wastewater Treatment

    Secondary Wastewater Treatment

    Secondary wastewater treatment is the 2nd stage of wastewater treatment that takes place after the primary treatment process.

     
    Spent Caustic Treatment

    Spent Caustic Treatment

    Spent caustic streams from refineries and ethylene production typically have a high chemical oxygen demand (20 - 500 g/L) and contain chemicals that are hazardous, inhibitory, and/or biorefactory.

     
     
    Tertiary Wastewater Treatment

    Tertiary Wastewater Treatment

    Tertiary treatment is the next wastewater treatment process after secondary treatment. This step removes stubborn contaminants that secondary treatment was not able to clean up.

     
    TOC Reduction for Wastewater

    TOC Reduction

    Trace organics are a key challenge facing the wastewater industry

     
     
    Wastewater Treatment Water Quality Analyzers and Process Control

    Water Quality Analyzers and Process Control

    Keep up with increased regulatory and quality control drivers that require better analytical and control techniques to stay within regulated, permitted and/or control limits. See how...

     
     
    © Siemens AG 2011 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID