Salt Lake Refinery Wastewater Treatment Upgrade Passes With Flying Colors 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Wastewater Treatment

Salt Lake Refinery Wastewater Treatment Upgrade Passes with Flying Colors

Challenge

The North Salt Lake (Utah) Refinery of Big West Oil LLC, a wholly owned subsidiary of Flying J Inc., needed to upgrade its wastewater treatment facilities to remain compliant with its wastewater discharge permit. The refinery had increased its throughput by more than 100% over the last 20 years without any major additions to the wastewater system. The larger wastewater flow resulted in less holding time to respond to upsets and increasing maintenance costs as a result of the refinery’s existing circular DAF unit’s age.

Solution

In 2006, refinery management decided to upgrade the 400 gpm (91 m³/hr)-treatment system. After a successful on-site pilot study, Siemens Water Technologies designed a new rectangular Folded Flow® DAF system that included an ancillary flocculation and flash mix tank. The new unit came online in May 2009.

The new design resulted in a smaller footprint that enhances separation and allows for better hydraulic loading at a higher rate for more effective removal of contaminants. The footprint is minimized by folding the effluent flow underneath the influent in the new DAF unit, allowing separation to occur over a surface area of 132 ft2 (12.3 m2) – less than a quarter of the surface area provided by the 27-ft (8.2-m) diameter circular tank. Dissolved air comes in with recycled water on the Folded Flow unit through a dispersion pipe that runs the full width of the tank – as opposed to being delivered in the middle of the tank with a dispersion tray as did the circular DAF unit.

Results

The new DAF system requires less maintenance and thus, less operator attention. It has also significantly improved the consistency and reliability of treatment. 

Comparing discharge data six months before and after the project, BOD levels in wastewater from the refinery fell by 67%, COD dropped 60%, and ammonia, BTEX and sulfate/sulfides experienced minor reductions.

This marks the first Folded Flow DAF separator to provide secondary oil/water separation in a U.S. refinery.

Full case study for download

top of page
Print
Contact Us
Folded Flow® Dissolved Air Flotation Separator
Get help now
Contact

Featured Products

Folded Flow® Dissolved Air Flotation Separator 
Oil-Water Separators

Featured Article
A Clean Conclusion - reprinted from January 2011 issue of Hydrocarbon Engineering

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID