New Polymer Feed System Provides Efficient Polymer Activation For Less Capital Outlay, Smaller Footprint 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Wastewater Treatment

New Polymer Feed System Provides Efficient Polymer Activation For Less Capital Outlay, Smaller Footprint

Challenge

The 1.5 million gallons per day (MGD) West Carrollton Wastewater Treatment Plant in West Carrollton, Ohio came on-line in 1989 and today serves 12,000 area residents. The activated sludge facility produces an average of 200 wet tons/month of sludge that, following belt filter press dewatering, is spread on area farmland by a biosolids management company. Polymer is added to the sludge prior to belt press dewatering to aid in liquid-solid separation.

After 13 years, West Carrollton plant management found it was time to replace the facility’s two-stage dry polymer feed system. “Our original system had served its useful life,” says Utility Superintendent Tom Scherack. “As with any older system, components were becoming worn out and its operation had become maintenance intensive. We also needed more room in the polymer mixing area and hoped to replace our old system with something smaller.” The old polymer feed system had served the West Carrollton plant well, but it was time for a change. “Basically, we were looking to maintain our same level of polymer performance but wanted a system that took up less space and, hopefully, required less capital outlay,” says Scherack.

Solution

A PolyBlend® M Series Polymer Feed System was installed in February 2002 at the West Carrollton facility.

  • The PolyBlend® is a liquid polymer feed system with a tapered mixing chamber that provides high performance polymer mixing and feed.


Results

The PolyBlend® feed system applies high mixing energy at the first contact of polymer and water for a short duration on initial shear. The system also applies mixing through a tapered regime, which minimizes polymer agglomeration and fracturing. After initial wetting or inversion in the high-shear impeller zone of the unit, polymer solution passes through a cylindrical processing zone where it is subjected to continuously decreasing shear rates over a period of time. The unit is equipped with “C” Controls functions, which along with a variable speed mixer offers a system with unmatched activation flexibility. The controller is capable of maintaining constant solution strength by sensing changes in incoming make-up water flow and automatically respond to these flow changes via a motor-driven control valve. Even primary and secondary dilution water are kept at the same ratio as output is adjusted.

  • After installation of the PolyBlend®, the ideal stroke and speed parameters for West Carrollton’s cationic polymer were established. “It’s a real simple operation,” says Scherack. “We found what stroke and speed the PolyBlend® needed to be set at and we just let it go.
  • West Carrollton’s new polymer feed system is in the same location as the old two-stage system but is mounted on the wall instead of taking up valuable floor space.
  • Since installation, the new feed system has required virtually no maintenance.
  • In addition, the cost of the PolyBlend® feed system was approximately 15 percent of the cost of a new, two-stage dry polymer feed system. “We got what we were looking for in a new polymer feed system,” says Scherack. “Our new PolyBlend® has a much smaller footprint than our old system, while still providing a high level of polymer activation and with no maintenance headaches. And, we got all this for a lot less cost upfront.”

top of page
Print
Contact Us
PolyBlend® M Series
Get help now
Contact

Related Products

PolyBlend® M Series

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID