Removal of Vanadium from Petcoke Leachate Waste 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Wastewater Treatment

Wastewater Ion Exchange Provides a Solution for Removal of Vanadium from Petcoke Leachate Waste

“Petcoke” is a byproduct of petroleum refining and consists largely of carbon and ash residuals from crude oil processing. Depending on the source of the crude, the ash in petcoke will contain low to significant concentrations of nickel, vanadium, iron and other metals.


Challenge

In January 2006, Siemens Water Technologies , formerly USFilter, was contacted by a California business that accumulates, stores and ships petroleum coke to its customers worldwide.  The petcoke at this customer’s site was originally stored in uncovered concrete vaults. During a storm, the rainwater would percolate through the petcoke, leaching nickel and vanadium from the ash in concentrations higher than discharge limits. The customer contacted Siemens to find a reliable, straight-forward treatment method to remove these metals from accumulated rainwater.

Solution

Siemens’ solution features our wastewater ion exchange (WWIX) service. Wastewater ion exchange is a service-based option which utilizes ion exchange resins and other medias selected to remove specific ionic contaminants from groundwater, industrial wastewater, and process water for recycle. DOT approved vessels containing the selected resin or media treat the water until the capacity is reached.  Once exhausted, the WWIX vessels are removed and replaced with fresh, DOT-compliant vessels and returned to service. Exhausted vessels are returned to our processing facility where the contaminants are removed from the media/resin.

The WWIX system supplied to the customer consists of two 30-cubic foot anion resin vessels in lead-lag configuration, followed by two 30 cubic foot vessels of selective cation or strong acid cation resin, also in lead-lag configuration. The anion resin targets the vanadium while the cation removes nickel.

Results

Once the existing volume of rainwater was treated and discharged, the customer was able to implement a smaller WWIX system for periodic maintenance of water. 

Siemens provided a fast, reliable treatment system that can be expanded or in this case, reduced as the customer’s needs change.  Off Site regeneration at Siemens RCRA facility provides the customer with an advantage of simple operation with compliance to all RCRA regulations while hazardous metals are recovered.


Download Full Case Study

top of page
Print
Contact Us
Wasewater Treatment Case Study
Get help now
Contact

Featured Products and Services

Wastewater Ion Exchange Services
Hazardous/Non-Hazardous Waste Treatment and Recycling
Ion Exchange Resins

Brochures
Wastewater Ion Exchange Service
Hazardous/Non-Hazardous Waste Treatment and Recycling

Treatment Applications
Hazardous Waste Removal in Wastewater Treatment
Dissolved Metals Removal in Wastewater Treatment

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID