Hazardous Waste Treatment 

Hazardous Waste Treatment 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Wastewater Treatment
    • Alkaline Cleaner Recovery
    • Archimedes / Screw Pumping
    • Biological Treatment
    • BOD & COD Reduction
    • Chemical Feed and Control
    • Clarification and Sedimentation
    • Disinfection
    • Dissolved Metals Removal
    • Hazardous Waste Treatment
    • Hexavalent Chrome Removal
    • Nutrient Removal
    • Oil and Water Separation
    • Primary Treatment
    • Secondary Treatment
    • Spent Caustic Treatment
    • Tertiary Treatment
    • TOC Reduction
    • Water Quality Analyzers and Process Control
  • Hazardous Waste Treatment

Hazardous Waste Treatment

In the past, hazardous waste management meant removing pollutants and disposing of residuals in a landfill. As industry and business have become more environmentally conscientious, and in order to comply with federal, state and local regulations, the need for alternatives to these historic methods has increased, and so has our ability to offer alternate solutions.

Central hazardous waste treatment and recycling facility in Minnesota

Hazardous wastes are generated as the result of treatment steps performed on industrial wastewaters prior to discharge, or contaminant-containing groundwaters.  In these cases, the treatment process (for example, by precipitation, evaporation, filtration, or ion exchange technology), produces a residual waste, including sludge and spent media, which must be analyzed, using the Toxic Characteristics Leaching Procedure (TCLP) test. The results of the TCLP are used to determine whether a waste is hazardous or non-hazardous.  

RCRA is the Resource Conservation and Recovery Act, a set of regulations adopted by Congress and administered by US Environmental Protection Agency (EPA), State and local regulatory agencies. RCRA defines what hazardous wastes are and how they must be legally stored, treated and disposed of. Many US states have been given authority by the EPA to enforce RCRA rules and also establish additional local and regional rules if necessary, however, State laws can never reduce the standards enacted by the EPA. There are significant legal liabilities to companies for not properly managing waste residuals according to RCRA regulations.

Waste may be classified as either Listed or Characteristic hazardous waste. RCRA regulations provide guidance to assist the waste generator in determining whether the waste falls into either classification.

With few exceptions, the EPA has classified the residuals from the following six manufacturing processes, also called Electroplating Processes, as Listed Hazardous Wastes which must be dealt with as such. The residuals from these processes are assigned the F006 hazardous waste code.

  • Electroplating
  • Coating (chromating, phosphating, coloring)
  • Electroless Plating
  • Chemical Etching and Milling
  • Anodizing
  • Printed Circuit Board Manufacturing

 

Other metal finishing processes performed in conjunction with the above 6 Listed electroplating processes are also considered F006 Listed Hazardous Wastes.

If any part of the resulting wastewater or waste residual which contains the following metals,  then the waste is a Characteristic Hazardous Waste:

  • Arsenic - 5 ppm
  • Chromium - 5 ppm
  • Mercury - 0.2 ppm
  • Barium - 100 ppm
  • Cyanides - 250 ppm
  • Selenium - 1 ppm
  • Cadmium - 1 ppm
  • Lead - 5 ppm
  • Silver - 5 ppm

 

Hazardous waste treatment involves almost anything that can be done to a hazardous waste prior to disposal.  Any method, technique or, process designed to change the physical, chemical, or biological character or composition of the hazardous waste, so as to neutralize the waste or to make the waste less hazardous and thereby safer for transport, increase potential for recovery, reuse or storage, or to reduce waste volume.

Waste dewatering is a efficient and effective treatment method used for waste volume reduction.  A variety of treatment systems are employed to dewater waste - including belt presses, centrifuges, and other devices.  Siemens offers a complete range of dewatering systems in a range of sizes and suitable for all forms of reuse applications - including land application, composting, and incineration.

Siemens Water Technologies owns and operates two, fully-permitted facilities with federal RCRA Part B and CERCLA authority and specializing in the treatment of inorganic wastes and wastewater. Wastes are sent to the facilities in drums (of all sizes), portable totes, cubic yard bags or boxes and tanker trucks. Virtually everything that we take into our facilities is in some way recycled. Recycling reduces liability, which is a significant incentive to many of our customers.

The heart of our hazardous waste treatment operations are in facilities located in Roseville, Minnesota and Los Angeles, California. These facilities serve as regional hubs for the treatment of hazardous waste and wastewater and the recovery of reusable by-products collected from the company’s hazardous waste customers. Siemens Water Technologies is the only company whose facilities handle and regenerate ion exchange resins and other media.

Our goal is to produce zero hazardous waste by extracting all reusable material, to eliminate pollutants from the environment and avoid disposal costs and liability. Most of the treatment residual wastes (F006, etc.) shipped to our facilities are inorganic or trace organicmaterials. Our advanced processing techniques have allowed us to increase beneficial reuse rate of these wastes to over 90% as reusable chemicals and metallic commodities.

Treatment Technologies for Hazardous Waste:

Sludge Dewatering
Waste Reduction & Recycle

top of page

Contact Us

For more information about hazardous waste treatment , contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Hazardous Waste Treatment Case Study

Microfiltration System Reduces Heavy Metal Waste by Two-Thirds

Marathon Norco Aerospace located in Waco, Texas is one of the few manufacturers of rechargeable, nickel cadmium batteries for the aerospace industry.  One of the production problems associated with the manufacture of rechargeable, nickel cadmium batteries is the use of a number of heavy metals.  Two of the metals which can be problematic when it comes to waste disposal are cadmium and chromium.

The amount of heavy metal waste generated at the Waco facility categorized the plant as a "significant hazardous waste generator," which created costly off-site hazardous waste disposal and extensive record keeping and documentation. Since 1972, the plant has used a diatomaceous filter system to reduce the volume and concentrate heavy metals in the waste. The plant's hazardous waste production required transport from the plant of over 100,000 pounds per year.

Read Full Case Study

top of page
Print
Contact Us

Featured Products and Services

Hazardous Waste Recycling and Treatment Services
Belt Filter Presses
Filter Presses
Sludge Dryers

Hazardous Waste Treatment Case Studies

Cooling Tower Blowdown Treated to Reach New NPDES Permit Levels
Microfiltration System Reduces Heavy Metal Waste by Two-Thirds
California Petroleum Refinery Seeks Assistance With Permit Violations for Stormwater Discharge to Waterway
Wastewater Ion Exchange Provides a Solution for Removal of Vanadium from Petcoke Leachate Waste

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID