Dissolved Metals Removal From Wastewater 

Dissolved Metals Removal from Wastewater 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Applications
    • Aquatic Water Treatment
    • Corrosion and Biofouling Protection
    • Drinking Water Treatment
    • Groundwater Remediation
    • High Purity Water
    • Industrial Process Water
    • Odor and Vapor Control
    • Oil & Gas Produced Water
    • Sludge & Biosolids Treatment
    • Wastewater Treatment
    • Water Recycle & Reuse
    • Water and Wastewater Library
    • Find a Case Study
  • Wastewater Treatment
    • Alkaline Cleaner Recovery
    • Archimedes / Screw Pumping
    • Biological Treatment
    • BOD & COD Reduction
    • Chemical Feed and Control
    • Clarification and Sedimentation
    • Disinfection
    • Dissolved Metals Removal
    • Hazardous Waste Treatment
    • Hexavalent Chrome Removal
    • Nutrient Removal
    • Oil and Water Separation
    • Primary Treatment
    • Secondary Treatment
    • Spent Caustic Treatment
    • Tertiary Treatment
    • TOC Reduction
    • Water Quality Analyzers and Process Control
  • Dissolved Metals Removal

Dissolved Metals Removal from Wastewater

Many industrial wastewaters contain dissolved metals as a result of their manufacturing processes.  Included among them are mercury, lead, cadmium, silver, copper and chromium.  Wastewater treatment systems are designed to reduce metal contaminants to meet discharge requirements and/or achieve the water quality level needed for reuse and recycling.   

Metals Removal System
Metals removal system featuring ion exchange technology

Many industrial manufacturing processes produce wastewaters containing heavy metals.  Industries include printed circuit board manufacturing, metal finishing, automotive, aerospace, semiconductor manufacturing, electroplated metal parts/washing, textile dyes and steel, to name a few.  As a result of improper treatment prior to discharge, many dissolved metals have been found in harmful concentrations in groundwaters which are destined for potable drinking water.  In small quantities, certain heavy metals are nutritionally essential for a healthy life, but large amounts of any of them may cause acute or chronic toxicity (poisoning).

The metals most often linked to human poisoning have links to learning disabilities; cancers and death are typically caused by copper, nickel, cadmium, chrome, arsenic, lead and mercury.  Many of these metals are required by humans in trace amounts, but in larger, persistent dosages, these heavy metals become toxic when they are not metabolized by the body and accumulate in the soft tissues. Heavy metal toxicity can result in damaged or reduced mental and central nervous function, lower energy levels, and damage to blood composition, lungs, kidneys, liver, and other vital organs.

The most commonly encountered toxic heavy metals include:

  • Arsenic
  • Lead
  • Mercury
  • Cadmium
  • Iron
  • Aluminum  

Other heavy metals of concern include:

  • Antimony
  • Chromium/chrome
  • Cobalt
  • Copper
  • Manganese
  • Nickel
  • Uranium
  • Vanadium
  • Zinc

In addition to concerns for human health and the environment, an increased desire to reuse and/or recycle industrial wastewaters also requires that metals removal occur in order to meet influent water quality requirement needed by the manufacturing process and equipment. 

Siemens can offer a wide range of treatment technologies depending on the specific contaminant to be reduced.

Ion exchange is a proven technology with effective treatment results for the removal of dissolved metals.  Siemens Water Technologies offers permanent, hard-piped ion exchange treatment systems containing contaminant-specific treatment resins, as well as removable systems.  Our service ion exchange approach integrates equipment and service option combinations, thereby minimizing a plant’s capital investment and reduces overall space requirements.  The system components are selected based upon available manpower, space limitations, access limitation and the specific water quality required.  Service ion exchange provides the ultimate flexibility to add or remove treatment capacity as your business grows or compliance limits change.  If needs change, we can simply change the media types and/or tank size, thereby saving our customers significant capital expense.

Once exhausted, the exchange vessels are removed and replaced with fresh, DOT-compliant vessels and returned to service. Exhausted vessels are transferred to our central treatment and processing facility where the hazardous/non-hazardous contaminants are removed from the media/resin.  Service ion exchange minimizes the need for handling and on-site storage of chemicals and wastes for improved safety and compliance at your site. This option also saves valuable manufacturing space while minimizing your maintenance and installation requirements.

Microfiltration technology also offers a cost effective and sustainable solution for removal of heavy metals in wastewater and for water reuse applications.  The membrane provides for an absolute barrier to the passage of solids and therefore is capable of removing metals (and other contaminants) to their solubility limits.  Siemens' Memtek® microfiltration system incorporates proprietary crossflow tubular membranes which remove precipitated contaminants and produce a high quality filtrate suitable for discharge, or for feed to a reverse osmosis unit or other polishing technology.

Dissolved Metals Removal Technologies for Your Wastewater Treatment Applications:

Ion Exchange
Physical/Chemical Treatment Systems
Microfiltration Membrane Systems 

top of page

Contact Us

For more information about dissolved metals removal in wastewater treatment, contact our Information Desk, Monday through Friday, 8 a.m. to 5 p.m., Eastern Standard Time: 1.866.926.8420 or 1.724.772.1402 or information.water@siemens.com.

top of page

Dissolved Metals Removal Case Study

Microfiltration System Reduces Heavy Metal Waste by Two-Thirds

Marathon Norco Aerospace located in Waco, Texas is one of the few manufacturers of rechargeable, nickel cadmium batteries for the aerospace industry.  One of the production problems associated with the manufacture of rechargeable, nickel cadmium batteries is the use of a number of heavy metals.  Two of the metals which can be problematic when it comes to waste disposal are cadmium and chromium.

The amount of heavy metal waste generated at the Waco facility categorized the plant as a "significant hazardous waste generator," which created costly off-site hazardous waste disposal and extensive record keeping and documentation. Since 1972, the plant has used a diatomaceous filter system to reduce the volume and concentrate heavy metals in the waste. The plant's hazardous waste production required transport from the plant of over 100,000 pounds per year.

Read Full Case Study

Dissolved Metals Removal
top of page
Print
Contact Us

Featured Dissolved Metals Removal Products and Services

Ion Exchange Systems
Neutralization Systems
Continuous Precipitation System (CPS)
Batch Precipitation System (BPS)
Memtek Microfiltration Systems
CuCMP Wastewater Treatment & Recycle
Chemical Reaction Systems
Chrome Reduction Systems
Replacement Ion Exchange Resins
Service-Ion Exchange
Hazardous/Non-Hazardous Waste Treatment and Recovery

Dissolved Metals Removal Case Studies

Ion Exchange Treatment of Regulated Metals in Coal Ash Found to be Efficient in Power Industry
Parker Hannifin, Formerly Aeroquip, Complies with Local Pretreatment Regulations
Using Microfiltration and Dewatering/Drying Equipment

Nevada Goldfield's Wastewater Treatment System Uses Reverse Osmosis and Ion
Exchange to Meet Stringent Metal Limits

Copper CMP/CMP Wastewater Treatment – A Classical Method with a Recycling Twist
Cooling Tower Blowdown Treated to Reach New NPDES Permit Levels
Microfiltration System Reduces Heavy Metal Waste by Two-Thirds
Hexavalent Chrome Treatment for Rinsewater Recycling Reduces Feedwater Demand and Wastewater Discharge
California Petroleum Refinery Seeks Assistance With Permit Violations for Stormwater Discharge to Waterway
Specialty Media Reduces Cadmium From Electroplating Wastewater Discharge 
Kentucky Municipal Wastewater Treatment Facility Chooses Siemens to Comply With Whole Effluent Toxicity (WET) Discharge
New Media Reduces Copper and Zinc From Hydrocarbon Processing Wastewater
New Media Removes Trivalent Chromium From Electropolishing Wastewater

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID