SIEMENS

 

MEMCOR® Submerged Membrane System Starts Up At Orange County Water District 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
      • Contact Us
      • Request A Proposal
    • Applications
      • Aquatic Water Treatment
      • Drinking Water Treatment
      • Groundwater Remediation
      • High Purity Water
      • Industrial Process Water
      • Odor and Vapor Control
      • Oil & Gas Produced Water
      • Sludge & Biosolids Treatment
      • Wastewater Treatment
      • Water Recycle & Reuse
      • Water and Wastewater Library
    • Water Recycle & Reuse
      • Disinfection
      • Water Quality Analyzers and Process Control

    MEMCOR® Submerged Membrane System Starts Up At Orange County Water District

    Challenge

    The Orange County Water District (OCWD) of Fountain Valley, California needed to increase its potable water supplies to meet the future water demands of this fast-growing area.  In 1997, the OCWD and the Orange County Sanitation District released a joint report proposing a groundwater replenishment project (GWRS) to serve the residents of Orange County.  The project would reclaim secondary treated wastewater, reducing the amount of wastewater discharged to the ocean, and providing a new local water source.  It would also improve the overall water quality in the groundwater basin by reducing the mineral content as well as preventing ocean water contamination. 

    Solution

    The OCWD has started up an advanced water treatment facility to provide 75 MGD (284 MLD) of reclaimed water for agricultural, industrial and indirect potable use.  Part of the GWRS, the water treatment facility consists of a MEMCOR® submerged membrane system from Siemens that supplies 87 MGD (329 MLD) of water to a reverse osmosis (RO) unit, followed by advanced oxidation (ultraviolet light plus hydrogen peroxide).  Orange County awarded the $27M microfiltration contract to Siemens in 2002 after extensive pilot and demonstration-scale testing of equipment from three membrane suppliers at OCWD’s previous 5-MGD (19 MLD) reclamation plant at the site, known as Water Factory-21. Orange County chose Siemens based on a life cycle cost analysis of the MEMCOR submerged membrane system.  The system is currently the largest in the Americas and one of the largest in the world. 

    Secondary treated wastewater that was formerly discharged to the ocean is treated with the submerged membrane system to remove all suspended solids, bacteria and other harmful contaminants.  The water is then pumped into recharge basins or barrier wells, where it is blended with other groundwaters, and then travels through the soil, which provides additional natural treatment of the water.

    Results

    The MEMCOR membrane system is composed of 26 compact units that provide more than five times the treatment capacity of a conventional clarification system housed in the same footprint.  It does not require chemical pretreatment except for pre-chlorination, and requires less maintenance and operator intervention.  The high-quality effluent increases the reliability, and reduces the capital and operating costs, of the downstream RO system.

    Each of the 26 units, or cells, contains 608 hollow fiber membrane modules.  The cells are arranged in four trains, each having a dedicated MemSAP (service access platform) to facilitate system maintenance.  Each cell is fitted with its own filtration pump that draws water through the membrane fibers.  The modules are arranged in racks, and sit 14 feet (4.3m) below the raw water elevation.  This allows the OCWD to make use of the hydraulic gradient, eliminating the need to pump water into the membrane cells.

     

     

     

    Microfiltration Building at Orange County Water District

    Submerged Membrane Cells

    Submerged membrane maintenance platform

    top of page
    Print
    Contact Us
    Membrane ground water replenishment system.
    Get help now
    Contact

    Related Product

    MEMCOR® Submerged Membrane System

    Download Case Study
    Full Case Study



    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID