Water
SIEMENS ARROW siemens.com 
country identifier
Home  |   Solutions  |  Products & Services  |  Parts & Support  |  About Us
Site Map  |   Contact Us
[Advanced]

Solutions

Applications
Technologies
Water and Wastewater Library

Water Technologies > Solutions > Applications
Drinking Water Treatment – Hydrogen Sulfide Removal
Hydrogen sulfide removal in drinking water is not carried out due to a health hazard but because hydrogen sulfide is a common nuisance contaminant whose distinctive "rotten egg" odor makes water treatment desirable.  Siemens provides H2S removal systems for municipalities.

Most methods for treating sulfur water rely on the oxidation of hydrogen sulfide gas into elemental sulfur, a solid. Oxidation is the process by which soluble or dissolved contaminants are converted to soluble byproducts or insoluble products that can be filtered. This process changes the chemical and physical properties of the reactants. Hydrogen sulfide can be oxidized by several methods. If concentrations exceed 6.0 mg/l, chemical oxidation such as chlorination is recommended. If concentrations do not exceed 6.0 mg/l and water pH is above 6.8, an oxidizing filter such as manganese greensand can be used.

Siemens Water technologies offers a range of processes to remove hydrogen sulfide from water:

Siemens also provides pilot treatment systems and analytical testing to document the efficacy of treatment prior to installation. We also provide parts and service on all of our equipment, as well as equipment which may have been provided by other manufacturers.

 Drinking Water Treatment and Services

Case Study: Midas OCM Field Testing Confirms Increased Capacity for H2S Adsorption and Odor Removal

Midas OCM (Odor Control Media) was developed using a special manufacturing process which enabled the media to have increased ability to adsorb H2S when compared with other odor control medias in the current marketplace.  Increased adsorption offers the benefits of longer run lengths, fewer bed replacements and minimal downtime. 

This unique and patented process converts H2S directly to elemental sulfur rather than sulfuric acid, which is the typical reaction of H2S on carbon.  Since the sulfur molecule is smaller than the sulfuric molecule, the carbon is able to adsorb a greater number of sulfur molecules.  By comparison, Midas OCM will last between 3 to 8 times linger than conventional medias used for this purpose.

 Full Case Study

Activated Carbon for Hydrogen Sulfide Removal

Drinking Water Hydrogen Sulfide Removal


Featured Products and Services
Contact Us Print

©  Siemens AG 2008 - Water Technologies, Corporate Information | Privacy Policy | Terms of Use | Digital ID