key visual
site identifier
SIEMENS ARROW siemens.com 
country identifier
Home  |   Solutions  |  Products & Services  |  Parts & Support  |  About Us
Site Map  |   Contact Us
[Advanced]

Solutions

Applications
Technologies
Water and Wastewater Library

Water Technologies > Solutions > Applications
Drinking Water Treatment - Conventional Water Filtration
Conventional water filtration is yet another way to treat drinking water. In the drinking water treatment process, water is filtered as the final step to remove remaining suspended particles and unsettled floc.  Conventional filtration eliminates these materials from the water stream, producing a purified drinking source. Clean drinking water is especially important for large organizations such as municipalities, and Siemens has a variety of conventional methods to suit drinking water filtration needs.

The most common type of conventional filters contain sand, activated carbon, or anthracite coal. These filtration media can remove organic compounds, which contribute to taste and odor.  Filters must be cleaned periodically, and this is accomplished as water is passed quickly upward through the filter, opposite the normal flow direction (called backflushing or backwashing) to remove embedded particles. Compressed air may be used to break up the compacted filter media to aid the backwashing process (air scouring). Backwashed solids are usually disposed of along with the sludge from the sedimentation basin.

Pressure filters work on the same principle as rapid gravity filters; the filter medium is enclosed in a steel vessel and the water is forced through it under pressure.

Siemens Water Technologies is a world leader in supplying all types of systems, components, and services for drinking water filtration. Our technologies include:

Siemens also provides pilot treatment systems and analytical testing to document the efficacy of treatment prior to installation. We also provide parts and service on all of our equipment, as well as equipment which may have been provided by other manufacturers.

 Municipal Drinking Water Treatment Technologies and Services

Case Study: Tri-Town Water District Expands Capacity While Decreasing Plant Footprint

The Tri-Town Water District serves the towns of Addison, Bridport and Shoreham, Vermont.  The original conventional water treatment plant was built in 1966 to treat surface water from Lake Champlain and produced an average of 765,000 gallons per day (2.8 MLD) with a peak summer demand of about 1,000,000 gallons per day (3.8 MLD). In 1999, the District hired Otter Creek Engineering Inc. to do an evaluation of the facility.  It was determined that the treatment system, particularly the clarification step, needed improvement; and the plant needed more capacity for future growth. The plant capacity was 1.1 MGD (4.2 MLD) and growth projections dictated they expand the plant capacity to 1.9 MGD (7.2 MLD). Accomplishing this task was more difficult since the site ruled out expansion to the existing plant footprint, and the owner needed to produce water during the construction phase of the project.

 Full Drinking Water Filtration Case Study

Drinking Water Filtration Case Study

Conventional Water Filtration Package Plant


Additional Information
Additional Information
Contact Us Print

©  Siemens AG 2008 - Water Technologies, Corporate Information | Privacy Policy | Terms of Use | Digital ID