SIEMENS

 

Case Studies 


Water Technologies

    X

    Contact


    search

    • Water Technologies
      • Products
      • Services
      • Parts
      • Municipal
      • Industries
      • Laboratory
      • Aquatics and Leisure
      • Applications
      • About Us
      • Site Map
      • Contact Us
      • Request A Proposal
    • Industries
      • Automotive
      • Environmental Remediation
      • Food and Beverage
      • Hydrocarbon Processing
      • Metals and Metal Finishing
      • Mining
      • Oil and Gas
      • Pharma
      • Power
      • Pulp and Paper
      • Semiconductor and Solar
    • Oil and Gas
      • Products
      • Case Studies
      • News Releases
    • Case Studies

    Oil and Gas - Case Studies

    Results 1 to 8 of 8

    Boiler Feed Water “Polished” With Mobile Demineralizer Trailers
    A refinery in Northern California was unable to meet its desired boiler feed water silica specifications on a consistent basis. The higher silica levels led to an excessive blow down requirement in the boiler system. The higher blow down rates were significantly affecting the refinery’s water, chemical, and natural gas costs.  More

    Cyanide Contamination at Manufactured Gas Plant Treated With Wastewater Ion Exchange Service
    Treatment system for cyanide remediation from prior manufacturing gas plant includes oil water separation, carbon filtration and wastewater ion exchange service  More

    Navajo Refinery Upgrades Wastewater Facility To Meet Clean Air Regulations
    The upgrade of the wastewater treatment systems will help Navajo Refining meet two U.S. Environmental Protection Agency regulations under the Clean Air Act  More

    OPTI Canada Uses Zimpro® Wet Air Oxidation System to Destroy Soot in Wastewater Generated During the Production of Syngas
    OPTI Canada Long Lake Project needed a system that would reduce costs associated with soot slurry landfill disposal and waste for their “next generation” oil sands development, which integrates established and proprietary technologies.  More

    PACT® System, Zimpro® Wet Air Oxidation Treat Variable Wastewater at Indian Refinery
    While producing a highly varied and variable wastewater that includes condensate from cracking, spent caustic liquor, and wastewater from other processes, the refinery had to meet all MINAS (Minimal National Standards) for effluent discharge.  More

    Repsol Chemical Treats Wastewater With PACT® and Wet Air Oxidation Systems
    The combination of wet air oxidation and PACT enables Spanish chemical plant to meet new wastewater discharge requirements, produce high-quality effluent.  More

    RO System Helps Discharge Regulations and Minimize Waste Volume
    In the Powder River Basin of Wyoming, Petro-Canada needed to treat the produced water from a Coal Bed Methane (CBM) project to meet discharge regulations and minimize waste volumes. CBM wells usually have to be dewatered to reduce pressure and allow methane gas to be released from the coal.  More

    Wastewater Ion Exchange Provides a Solution for Removal of Vanadium from Petcoke Leachate Waste
    In January 2006, Siemens Water Technologies , formerly USFilter, was contacted by a California business that accumulates, stores and ships petroleum coke to its customers worldwide. The petcoke at this customer’s site was originally stored in uncovered concrete vaults.  More

    1
    top of page
    © Siemens AG 2009 - Water Technologies
    Corporate Information | Privacy Policy | Terms Of Use | Digital ID