Flue Gas Desulfurization Wastewater Treatment 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Power Industry
    • Boiler Feedwater
    • Condensate Polishing
    • Cooling Tower Make-Up Water
    • Flue Gas Desulfurization
    • Pretreatment Solutions
    • Case Studies
  • Flue Gas Desulfurization

Flue Gas Desulfurization Wastewater Treatment

Siemens Water Technologies offers a complete treatment solution for flue gas desulfurization (FGD) wastewater, ensuring that power plants meet their water discharge requirements as they retrofit stations under the Phase 2 of the Clean Air Act amendments.

This solution includes engineering design, equipment supply, installation, checkout, startup, commissioning, operation, maintenance, financing or build-own-operate-maintain (BOOM) / build-own-operate-transfer (BOOT).
top of page

We combine several proven technologies to achieve a well functioning, integrated FGD treatment facility with appropriate performance guarantees, including:

  • Lime neutralization / desaturation
  • Heavy metal removal, including hard-to-remove priority species
  • Clarification
  • Filtration
  • Sludge thickening and dewatering
  • BOD / COD reduction
  • Nitrates and ammonia reduction
  • Selenium reduction
  • Mercury removal

Scrubber Technology

Scrubbers are used in U.S. power plants to meet air quality emission standards set by the U.S. Environmental Protection Agency (EPA) and by individual state requirements.  Recent updates to the regulatory programs call for further reduction of sulfur dioxide (SO2) emissions from coal-burning power plants.

FGD systems use either dry or wet scrubbers. Dry scrubbers generally use lime or limestone as a reagent to remove SO2 and although they use water in the process, the water usage is lower than with wet scrubbers. When the power plant's coal contains less than 2% sulfur, as it does in western coals such as the Power River Basin (PRB) coal, the plant will typically consider using dry scrubbers. Wet scrubbers are preferred when the coal contains higher amounts of sulfur. Since a power plant being retrofitted with a new FGD system will be in service for 25+ years, a number of power plants are installing wet scrubbers, even if they are currently using low sulfur coal, to have the future flexibility to use coals from many different world sources that may have higher sulfur content.

Wet FGD systems most commonly are of the limestone-forced-oxidation (LSFO) type to convert SO2 in the flue gas to gypsum. While this allows greenhouse gases to be released to the atmosphere, it removes the SO2 that causes acid rain.  Future versions of FGD systems will capture CO2 and dispose of it in an environmentally-friendly way.

Wet FGD scrubbers use an absorber tower in which flue gas is contacted by limestone slurry, resulting in conversion of SO2, in the flue gas into calcium sulfate (gypsum), with carbon dioxide (CO2) going up the stack.  Gypsum can be sold to wallboard manufacturers, thus turning a waste stream into a usable resource. To maintain required conditions in the scrubber (to control chlorides levels consistent with the scrubber’s materials of construction and to maintain ash fines levels low enough to maintain gypsum quality), a constant purge stream is discharged from the scrubber system.

The proper design of sludge dewatering systems and the selection of materials of construction are critical in FGD wastewater installations. Both of these key design areas can have a major impact on the treatment plant’s operation, reliability and cost.  Siemens Water Technologies has extensive expertise in FGD wastewater treatment and is the industry leader.  By having early discussions with the utility about their specific power plant, we are able to provide an optimized system at the best cost / benefit ratio.

Mercury Removal

Siemens is continually working on new mercury reduction technologies to reduce mercury levels below 12 parts per trillion (ppt).  These technologies are currently under evaluation and in pilot testing at various facilities nationwide.  For additional information on low level mercury removal please contact Adam Szczesniak, e-mail: adam.szczesniak@siemens.com.

top of page
Print
Contact Us

Contact Us

Jeff Gutierrez
1.480.706.1022
Send Email
Request a Proposal

Not all products and services are available in all parts of the world. Contact us to discuss your needs.

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.

Technical Papers

Wastewater Treatment for FGD Purge Streams
Duke Energy Carolina LLC’s Strategy and Initial Experience of FGD Waste Water Treatment Systems

© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID