A Package Plant Approach to Decentralized Wastewater Treatment 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Products
    • Activated Carbon
    • Aeration
    • Biological Treatment
    • Chemical Feed and Disinfection
    • Controls, Instrumentation and Analyzers
    • Conventional Filtration
    • Ion Exchange
    • Laboratory Water Products
    • Liquid and Vapor Phase Odor Control
    • Membrane Filtration & Separation
    • Physical/ Chemical Treatment
    • Separation and Clarification
    • Sludge and Biosolids Processing
    • Specialty Products and Accessories
  • Biological Treatment
    • Integrated and Advanced Biological Wastewater Systems
    • Jet Aeration Systems
    • Membrane Biological Reactor Systems (MBR)
    • Sequencing Batch Reactor (SBR)
    • Wastewater Mechanical Aeration Systems
    • Wastewater Package Treatment Plants
    • Wastewater Trickling Filter Distributors
  • Membrane Biological Reactor Systems (MBR)

A Package Plant Approach to Decentralized Wastewater Treatment

Decentralized wastewater management is defined as the collection, treatment, and reuse of wastewater at or near the point of waste generation.  Decentralized wastewater treatment has been utilized for many years using a number of different treatment technologies, most notably septic systems. 

In cases where septic treatment is not adequate to meet the treatment objectives, engineers will often incorporate secondary and tertiary treatment into the process design.  Attached growth, activated sludge or hybrid systems can all be used in combination with tertiary filtration and disinfection to achieve even the tightest effluent limits.  One technology that has proven very successful for decentralized systems in recent years is the membrane bioreactor (MBR).

The MBR technology incorporates settling, activated sludge, and filtration into a compact process configuration.  Membrane filtration is the distinguishing element of an MBR process.  Many different types and configurations of proprietary membranes exist, with most membrane manufacturers and several system integrators offering package or modular MBR systems.  These systems have a service range from a single residence to small communities or commercial establishments.  For this article, the authors are defining a package plant as a system that is fully assembled (wiring/plumbing) with the ability to start up and wet test all equipment, including electrical works, in the factory.  Due to shipping constraints, portions of the package plant may require re-assembly at the installation site.

There are several advantages to using package MBR systems over conventional treatment systems.  These include reduced engineering and construction labor as well as reduced installation and commissioning time.  Package MBR systems have a very small footprint and are capable of being assembled to meet tight project schedules.  Such systems also consistently produce effluent that can meet very stringent effluent limits and almost any re-use standards.  Package MBR systems also require less operator attention, and are easier to monitor remotely due to instrumentation and controls. 

Conversely, the main disadvantages of package MBR systems include their higher capital cost and energy demand.  The membranes also require periodic chemical cleaning, and the hydraulic limitations of the membranes might necessitate more system equalization. 

Xpress™ Package MBR System

Siemens Water Technologies is both a membrane manufacturer and package MBR system integrator.  The company’s Xpress™ package MBR system, which is illustrated through the examples that follow, is manufactured in four sizes.  The smallest unit has a treatment capacity of approximately 100,000 L/day and the largest has a treatment capacity of nearly 400,000 L/day average daily flow of domestic sewage.  The package plant includes fine screening, suspended growth biological treatment, and membrane filtration.  Ultraviolet disinfection can easily be added to these systems for complete treatment.  Each of the package plants undergoes up to two weeks of factory testing to ensure all mechanical and electrical works operate as designed prior to shipment. 

Grey Eagle Casino

The Grey Eagle Casino was a new commercial venture by the Tsuu T’ina Nation in partnership with Sonco Gaming (Alberta) Ltd.  This casino and future hotel/entertainment project is located on Tsuu T’ina lands in southwest Calgary, Alberta.  The location was unserved by water and sewer and had tight standards for discharging wastewater that ultimately goes into Pine Creek.  Any discharge at this location required advanced treatment including a highly filtered effluent with nitrogen removal to levels below 10 mg/L total nitrogen and phosphorus removal to levels less than 0.5 mg/L.  In addition to advanced treatment, the site layout arrangement required a compact system that would allow both the wastewater treatment and water treatment systems to be housed in the same building.  The equipment’s close proximity to the casino made stringent odor control necessary.  A very tight project schedule as well as the short supply of construction labor during a period of heavy oil field development made a simple, prefabricated system that could be set and installed quickly and inexpensively preferable. 

After looking at several options, Sonco Gaming’s engineer selected the Xpress MBR package plant.  With an estimated average flow rate of 200,000 L/day, the Xpress MBR plant addressed all of the casino’s specified needs.  The advanced treatment unit easily meets the casino’s stringent effluent requirements.  The system was designed with a completely enclosed biological reactor and covered membrane tanks.  A simple carbon adsorption odor control system ensures nuisance-free operation.  A compressed schedule necessitated that the building for the water and wastewater equipment be built well in advance of equipment delivery.  When the MBR skid arrived, it was conveniently lifted through removable roof panels, set in place, and quickly installed.  The complete wastewater system includes an in-ground equalization and sludge storage basin, lift pumps, and MBR package system (fine screen, anoxic and aerobic biological treatment reactors, and a two-cell membrane system followed by disinfection).  The effluent is discharged to a subsurface disposal system and ultimately drains into Pine Creek.  The system has been meeting all discharge requirements since it became operational in October 2007.

Lower Kuskokwim School District

The Lower Kuskokwim School District (LKSD), headquartered in Bethel in southwestern Alaska, is one of the state’s largest rural school districts.  LKSD services a 58,900-square kilometer area, roughly the size of the state of West Virginia.  With only 3,800 students, the LKSD operates several small, very remote sites.  Many of the wastewater treatment systems are on-site decentralized systems. 

Recently, the LKSD began to implement district-wide upgrades to its schools’ wastewater treatment systems.  Package treatment plants were recommended for three of the more remote schools that were evaluated.  A compact system was specified since the water and wastewater systems had limited space available. The LKSD also has a district-wide SCADA system that monitors many critical elements of its schools’ operations, including the wastewater treatment systems. 

The LKSD worked closely with its engineer and determined that a 100,000 L/day Xpress MBR package plant would best meet the district’s needs.  The solution met all critical design elements: small footprint, remote monitoring capability, and packaged system approach.  Since the three schools were very remote, the contractor elected to pre-construct a building around the Xpress system to simplify installation.  The unit was shipped from the factory in Thomasville, Georgia, to Billings, Montana, for full assembly.  The building was then deconstructed for shipping to Seattle, Washington.  The Xpress unit and building components were then loaded onto a barge and shipped to each school site which were all accessible by waterway.  The Xpress unit and building were off-loaded from the barge and reconstructed at the site.  So far, one plant has been commissioned and the other two are scheduled for commissioning this Winter.

Summary

Decentralized systems have been used for many years to meet a variety of project requirements.  MBR systems offer many unique advantages over more conventional wastewater treatment systems, and packaged MBR systems are a proven alternative for decentralized treatment.  Siemens has designed and manufactured the Xpress MBR package system for decentralized treatment since 2004 and to date has designed, constructed, and delivered nearly 30 such projects.

top of page

Print
Contact Us
 

Recommended Links

Xpress™ MBR Package Plant
MBR Technology
Wastewater Package Treatment Plants
Watewater Treatment Applications

Download White Paper

A Package Plant Approach to Decentralized Wastewater Treatment (pdf)

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID