Disc Filters in the Last Decade 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Products
    • Activated Carbon
    • Aeration
    • Biological Treatment
    • Chemical Feed and Disinfection
    • Controls, Instrumentation and Analyzers
    • Conventional Filtration
    • Ion Exchange
    • Laboratory Water Products
    • Liquid and Vapor Phase Odor Control
    • Membrane Filtration & Separation
    • Physical/ Chemical Treatment
    • Separation and Clarification
    • Sludge and Biosolids Processing
    • Specialty Products and Accessories
  • Conventional Filtration
    • Bag Filters and accessories
    • Cartridge Filters and Accessories
    • Cloth Type Filter Systems
    • Filter Housings and accessories
    • Gravity Filter Systems
    • Media - GFH,Greensand, Walnut Shell & Specialty
    • Packaged Water Treatment Plants
    • Parts and Accessories
    • Pressure Filter Systems
  • Cloth Type Filter Systems

Disc Filters in the Last Decade

Over the last decade, disc filters have been increasingly used in North America for municipal tertiary treatment, recycle/reuse, retrofit of conventional filters, and process water filtration.  Elsewhere, they are also used for pretreatment of ultrafiltration (UF) membranes, product recovery, and industrial reuse.  The difference in woven filtration media and flow pattern makes each type of disc filter unique to each application.

The two main disc filter techniques are outside-in and inside-out, which refer to the filter unit’s flow-through scheme.  Both techniques traditionally rely on filtration mediums that are configured in a flat panel design.  Although different in material and construction, both filter mediums produce a pretty consistent effluent quality. 

Outside-In Configuration

The outside-in flow scheme is one of the earlier disc filter techniques used in North America.  In this scheme, the discs are completely submerged.  Solids are filtered on the outside of the filtration medium while filtrate is collected inside a drum and conveyed out of the system.  Accumulated solids are removed by reversing a portion of the filtrate flow through a shoe attached to the medium while simultaneously rotating the whole drum/disc or just the backwash shoe on the stationary disc assembly. 
  
Solids are captured and held by the randomly spaced and sized nylon fibers that comprise the pile cloth filtration medium.  The cloth medium covers a honeycomb-shaped structure that is assembled around the filtrate drum/conduit. 

There are several drawbacks to this technology.  First, solids can sometimes pass through the pile media during high-pressure cleanings.  Second, the medium matrix is constantly submerged in an ever-increasing concentration of feed solids, making it difficult for the backwash shoe to keep it clean.  As a result, sludge withdrawal systems and additional high-pressure washing arrangements are frequently used in conjunction with these filters, sometimes further complicating the overall system.  Third, biological matter can also grow on the filtrate side of the filtration cloth, especially in unchlorinated filter feed/secondary effluents.  Fourth, to initiate the high-pressure backwash cycle and to expose the spray nozzles, the filtration process must be taken offline.  This can result in excessive tank drainage, lengthy rinse periods, and substantial reject volumes, as well as redundancy requirements for ensured continuous wastewater treatment.

Inside-Out Configuration

The inside-out filtration technique addresses many of the outside-in technique’s inadequacies.  The former reverses the flow pattern by feeding the filtration medium from the inside, and partially submerging the outside of the medium in filtered water.  Wastewater enters a central drum/conduit, where it is fed to the inside face of the filtration panels, which are assembled in a disc pattern around the drum.  Solids are deposited on the inside face of the medium, while filtrate is produced on the outside.  Backwash is initiated by headloss and is effected by high-pressure nozzle sprays that dislodge accumulated solids, propelling them back towards the inside.  After being collected in a trough inside the drum/conduit, the solids are conveyed out of the system by gravity.  The backwash spray is pulled from the same reservoir of product filtrate water in which the disc/drum assembly rotates.

The medium is a woven polyester cloth with an absolute-micron size rating that helps retain particles larger than the cloth opening size, as well as those greater than the available opening of the accumulation in the medium.  For tertiary reuse, this rating is typically 10 µm.  This medium is assembled in filter panels, which are inserted into plastic boxes that surround the feed drum/conduit in a disc configuration.  Each disc is composed of 28 filter panels.  Since the discs are in filtrate water only, there is no need for sludge removal mechanisms, resulting in a much simpler system. 

All of the above factors contribute to the inside-out disc filter’s better sustainability and lifecycle cost, compared to the outside-in configuration.

Flat vs Pleated Filtration Panels 

Both the inside-out and outside-in techniques rely on filtration mediums configured in a flat panel design – the pros and cons of which have been enumerated above.  In 2006, Siemens Water Technologies released an inside-out configuration disc filter with an innovative woven polyester pleated panel design.  This design increases the available effective filtration area (and thus, treatment capacity) by 40% over flat panel designs.  Pleated media is also structurally more durable and can easily withstand much higher headloss conditions than other media configurations.

The pleated media panels are a molded one-piece construction with structural stiffeners through the center of the panel area.  This panel configuration is more resistant to cloth deformation and the eventual tearing common to cloth stretched in flat panel designs.  No epoxy glue is used, eliminating the probability of cloth delamination.  The pleated media design also offers quick-release cleaning, helping improve the cleaning process and prevent media wear.

The filtration boxes (the filtration panels’ housing) are designed to be trash tolerant.  Unlike existing flat panel technology, the Forty-X disc filter’s filtration boxes do not contain internal gussets.  This allows large inorganic material such as plastics, algae strings, rags and other floatables to flow through and be rejected from the system and to not accumulate and affect the internal hydraulics of the filtration panels.

Water pressure-assisted seals and stainless steel sliding covers make accessibility and maintenance easier.  Leak points inherent in flat panel designs are minimized in the pleated filtration panel’s seals by using water column pressure.  The sliding cover design of the disc/drum’s internal assembly eliminates the need to lift a heavy cover – a benefit especially for outside installations in windy areas.

The disc filter’s higher filtration surface area, combined with its stronger configuration, results in a high throughput capacity, better feed distribution, and fewer backwash frequencies.  The disc filter’s design also serves as an ultimate barrier for suspended solids in tertiary treatment processes. 

Ideal Applications

The Siemens modular design offers flexibility for a broad range of flows and applications including water reuse, tertiary filtration and process water filtration.  The Forty-X disc filter’s modular and all-inclusive design allows for an easy and economical retrofit to existing structures.  The Forty-X disc filter has also received Title 22 approval, meaning it complies with the existing State of California Water Recycling Criteria that requires filtration technologies to reliably meet specific performance parameters for wastewater reuse applications.

Following are a few examples of how the Forty-X disc filter is helping facilities around the world:

New Zealand

A facility upgrade was necessary to address growth and new consent decrees.  But space constrictions prevented adding more concrete-style traveling bridge filters to the plant design.  The existing traveling bridge filters were swapped out for Forty-X disc filters.  The facility installed two of these disc filters in half the space of the traveling filters, to increase plant capacity.  Enough space is available in the concrete structure for more disc filter units to be added if future plant capacity increases are required.

Qatar, U.A.E
 
A multinational petroleum venture in the U.A.E. needed to treat its process water for reuse.  Water availability and space limitation were also factors at the facility.  One stream had domestic wastewater components and only required typical tertiary treatment to comply with reuse standards, while the other required further treatment by UF membranes in order to be reused in the facility.  The Forty-X disc filter’s space-saving design was a good fit.  The absolute micron rating of the woven polyester cloth in the filtration panel allowed consistent effluent quality, despite the variation of the influent concentration.  This allowed both an increase in flux and a decrease in UF Clean in Place (CIP) events, resulting in a more economical and sustainable operation.

Pennsylvania, USA

A sequencing batch reactor (SBR) facility that had an improperly functioning slow sand filter needed to improve its Total Suspended Solids (TSS) removal.  The solution was a “plug and play” installation consisting of a Forty-X disc filter placed on top of the existing SBR equalization tank.  The disc filter’s small footprint saved the facility additional civil work, all within the plant’s hydraulic profile that included existing ultraviolet (UV) disinfection equipment.  The unit was installed with water heaters to prevent winter freezing, which saved the additional expenditure of a building enclosure.

China

One of Wuxi, China’s major wastewater treatment facilities needed to upgrade but had little space available.  As there was no room to include a filtration step, Siemens retrofit the existing concrete chlorine contact chamber with Forty-X disc filters and UV disinfection.  Both the shallow profile of the Forty-X disc filter and the 600 sq.m (1234 sq.ft.) of surface area available in the filters’ pleated configuration, allowed expansion of filtration capacity and inclusion of UV disinfection in the existing concrete chlorine basin footprint.

top of page

Print
Contact Us
 

Recommended Links

Forty-X Disc Filter
Ultrafiltration Membranes
Tertiary Wastewater Treatment

Download White Paper

Disc Filters in the Last Decade (pdf)

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID