Capabilities 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Municipal
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Products
    • Activated Carbon
    • Aeration
    • Biological Treatment
    • Chemical Feed and Disinfection
    • Controls, Instrumentation and Analyzers
    • Conventional Filtration
    • Ion Exchange
    • Laboratory Water Products
    • Liquid and Vapor Phase Odor Control
    • Membrane Filtration & Separation
    • Physical/ Chemical Treatment
    • Separation and Clarification
    • Sludge and Biosolids Processing
    • Specialty Products and Accessories
    • Wastewater Treatment Solutions
    • Complete Water and Wastewater Treatment Solutions
  • Sludge and Biosolids Processing
    • Belt Filter Press
    • Composting
    • Digesters and Gas Storage
    • Filter Press
    • Gravity Sludge Thickeners
    • Sludge Dryers
    • Sludge Removal Equipment
    • Solids Reduction Process
  • Filter Press

How the J-Vap® System Works

The J-VAP® Dewatering/Drying System marries a specially designed diaphragm plate filter press with a unique vacuum/evaporation technology.

The technology consists of a filter press in which the dewatering and drying of slurry occurs and an energy conversion module that supplies heated water.  The heated water is used to heat the filter press and also includes a vacuum system used during the drying stage of the cycle. 

During the first stage, slurry is pumped into the chambers where the initial dewatering takes place and much of the free liquid is removed.  The J-Vap® system is a variable volume filter press; therefore, shorter feed cycle times may reduce the total cycle time.

After the initial filtration cycle, the vacuum/drying cycle begins. The chambers are heated with 180°F water and a vacuum is pulled. This causes the water remaining in the cake to evaporate at a lower boiling point.

The drying time can be adjusted to achieve the desired solids output. Virtually all the water in the cake can be removed prior to cake discharge. The same level of cake solids is easily duplicated during subsequent cycles.

Once the drying cycle is complete, the press is opened, the chambers are separated and the dried cakes are discharged.  The low moisture content provides excellent cake release; in most cases the solids literally fall from the chambers as they are opened. Cake removal from the system is clean and efficient.

See diagram here

top of page

Print
Contact Us
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID