Water Plant Rehabilitation and System Upgrades 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Services
    • Carbon Media Services
    • Ion Exchange Resin Services
    • Membrane Services
    • Mobile and Temporary Services
    • Retrofit/Rehab Services
    • Service Contracts
    • Testing Services
  • Retrofit/Rehab Services

Water Plant Rehabilitation and System Upgrades

Fiscal budgets continue to tighten in these rough times.  Monies for water plant expansions often are postponed or cancelled while demands for increased water quantities and quality never seem to end.  Rather than expanding plants or building new ones, many communities are rehabilitating or upgrading existing plants and filters to meet water demands.  Extending the life of a 20, 30, or even 40 year old plant has become a matter of necessity rather than a matter of choice.   Often, proper rehabilitation and system upgrades can extend the useful life of these plants for another 20 years.

Many existing water plants are able to increase output and improve quality by performing system upgrades.  Water sources vary as much as the communities they serve; thus, each individual plant upgrade must be reviewed as a unique opportunity.  Proper plant operations -- and the operators that keep those plants running -- are the number one resource available to optimize output.   Although many feel that water technology has become a science, there are plant supervisors using very creative methods to optimize their plant’s performance on a daily basis.  Giving qualified operations staff the tools to carry out preventive maintenance and proactive rehabilitation of equipment is essential to the plant’s longevity.  Maintaining structural integrity of the filters is a matter of necessity rather than convenience. 

When filters need rehabilitation or upgrades, often the filters and their components have to be taken off line for a period of time in order for these changes to be performed.  Plants that do not have the luxury of low-demand seasons or alternate water sources may need to rely on temporary mobile facilities to produce water during filter rehabilitation.  These mobile systems can be housed in a trailer, as shown in Figure 1.  The temporary plants can be mobilized and hooked up to the system, when necessary, to produce water for the community.  This allows bypassing the existing water system for a period of time while it is rehabilitated.



Utilizing qualified engineers, contractors and reliable vendors is essential to ensure that the work performed will endure for the foreseeable future.  As an example, many steel structures or equipment have not been properly cared for over the years and the inevitable rust has deteriorated their integrity.  An example of this is shown in Figure 2. A contractor who understands, and has had experience dealing with corrosion and its repair, is essential to proper rehabilitation.  Often, deteriorated plants can be restored to a useful life with proper rehabilitation.  The decision to rehabilitate a steel structure depends heavily on the integrity of the steel plate.  Even though many steel tanks have not received the proper preventative maintenance and are severely rusted, ultrasonic thickness testing meters are available to aid in determining the structural worthiness of the steel.  In many cases, steel structures that aesthetically look like they are in very poor condition can be brought back to life with proper surface conditioning and repainting.



Controls

The most popular upgrade to aging systems has been replacing the original control panel.  Upgrading from old cams, timers, or MS DOS supported Programmable Logic Controllers (PLC’s) to newer PLC’s with a Human-Machine Interface (HMI) (Figure 3) allows the operator flexibility in programming filter functions that optimize the filtration cycles.  With updated PLC’s and controls, the qualified operator has the ability to perform Design of Experiment (DOE) testing to optimize filter function, rather than having to rely on timed cycles or preset limits.  New control systems turn filter function optimization from chaotic trial and error to a user friendly optimization schedule.  Adding a Supervisory Control and Data Acquisition (SCADA) interface adds to the ease of remotely manipulating filter functions and data acquisition.  It also allows filter operation, alarm monitoring, and filter data and history accumulation to be accomplished remotely.



Filters

Reconditioning the filter section not only allows the operating life to be extended, but may also optimize and even increase filter performance.  Since filter backwash is a major source of wasted effluent water and loss of filter production time, optimizing the filter function to increase efficiency has become a key focus.  Rather than simply extending the time of the filter cycle between backwashes, the filter backwash cycle can be set to trigger on headloss or turbidity, which also aids in optimizing filter performance.

The addition of an air scour sequence to the filter backwash function greatly increases the cleaning potential of the filter bed during backwash.  Air scour through direct retention underdrains has several advantages.  Direct media retention underdrains (Figure 4) eliminate the need for support gravel that encases “pipe and lateral” underdrain designs; therefore, only the media (anthracite, sand, and garnet) needed directly for filtration is used.   Air is introduced by a high volume, low pressure blower through the underdrain to aid in the fluidization of the media during backwash.  This method is superior in cleaning the media during backwash, resulting in longer filter runs. Thus, there is less waste and more plant productivity.



Once filter operation is maximized, working to optimize the clarification and settling functions can potentially reduce the turbidity that is entering the filter bed section, thus extending the time between backwashes.

Clarifiers

Clarifiers are often the first filtration step in significantly reducing turbidity prior to final filtration stages.  Retrofitting or rehabilitating the clarifier section with improved, more efficient, or clean media reduces the amount of the turbidity passed on to the filter bed.  Improving clarifier efficiency and eliminating clarifier disruptions, such as turbidity break-through, significantly reduces the need to backwash the filter bed, thus improving filtration operation and efficiency.

For flashy water sources that frequently see high turbidity spikes, adding tube settlers prior to the clarifiers eliminates the operational strain on the clarifiers, thereby reducing system waste.  Many facilities are adding tube settlers to existing basins or adding new tube settling equipment prior to the clarifiers to reduce water turbidity early in the overall filtration process.

Filter to Waste

Adding a filter-to-waste sequence after the filter backwash cycle typically reduces the amount of turbidity that enters the clearwell directly after a backwash.  Directing effluent discharges temporarily to waste until optimal turbidity levels are achieved prevents turbidity spikes from entering the clearwell.  It also reduces the possibility that very high turbidity spikes, from filer malfunction, will enter the clearwell.

Ultraviolet (UV)

UV disinfection lamps (Figure 5) introduced into the filter effluent stream are very effective in disinfecting the water and helping to control the level of Disinfection Byproducts (DBP’s) in the distribution system. Unfortunately, these retrofits are often very difficult to install.  This is especially important since most filter effluent piping efficiently discharges directly to clearwells.  In addition, many facilities have limited space available between the end of the filter and external facility walls.  Because of these design configurations, retrofitting UV mechanisms to effluent discharge piping becomes a challenge.  Complex piping changes are typically needed to install the UV mechanism.  This is compounded even more if system redundancy is required.  

Conclusion

Retrofits, rehabilitation, or upgrades to existing facilities range from very simple adjustments to major system reconfigurations.  Depending on the level of upgrade, making sure that qualified engineers, contractors, and/or vendors are involved early in the planning will allow a smooth transition.   The goal is to end up with the highest quality water delivered from a highly efficient facility. 

top of page

Print
Contact Us
 

Recommended Links

Retrofit / Rehab Services
Mobile and Temporary Services
SCADA
UV Disinfection
Clarifiers

Download White Paper

Water Plant Rehabilitation and System Upgrades (pdf)

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID