How Does CEDI Work? 

Video: How Does CEDI Work? 

Water Technologies
  • English
X

Contact


search

  • Home
    • Product Groups
    • Market-specific Solutions
    • Investor Relations
    • Press
    • Jobs & Careers
    • Sustainability
    • About Us
    • Industry Sector
    • Energy Sector
    • Healthcare Sector
  • Market-specific Solutions
    • Automotive
    • Chemicals
    • Construction and Real Estate
    • Finance
    • Food&Beverage
    • Machine Building
    • Metals & Mining
    • Oil & Gas
    • Pharmaceuticals
    • Public Sector
    • Pulp & Paper
    • Tourism & Leisure
    • Transportaion & Logistics
    • Water
    • Wholesale / Retail
    • Cross Market Offerings
  • Water Technologies
    • Products
    • Services
    • Parts
    • Food and Beverage Industry
    • Life Sciences Industry
    • Marine Industry
    • Mining Industry
    • Oil and Gas Industry
    • Power Industry
    • Semiconductor and Solar Industry
    • Drinking Water Treatment
    • Municipal Wastewater Treatment
    • Aquatics and Leisure
    • Applications
    • About Us
    • Videos
    • Site Map
  • Videos
    • Aquatic Water Treatment Videos
    • Corporate Capabilities Videos
    • Corrosion and Biofouling Protection Videos
    • Drinking Water Treatment Videos
    • High Purity Water Videos
    • Sludge and Biosolids Treatment Videos
    • Wastewater Treatment Videos
    • Water Recycle and Reuse Videos
  • High Purity Water Videos

Video: How Does CEDI Work?

Siemens’ patented Ionpure CEDI technology removes ions from water using a unique combination of ion exchange membranes … ion exchange resins, … and electricity.

top of page

Transcript: How Ionpure Works

In the Siemens portfolio, the Ionpure name is known as a leading provider of innovative products for system integrators worldwide such as: Continuous Electro-Deionization … or CEDI … for chemical free production of Deionized water.

Siemens’ patented Ionpure CEDI technology removes ions from water using a unique combination of ion exchange membranes … ion exchange resins, … and electricity.

The ion exchange resins are continuously regenerated … without the need for regeneration chemicals.

To understand how the patented Ionpure CEDI technology actually works, let’s go down to the molecular level and take a look at some water containing ions.

Water contains positively-charged cations, represented by plus signs, and negatively-charged anions, represented by minus signs.

When a pair of electrodes is inserted and an electrical current applied, the electric field drives the cations in the direction of the cathode and, at the same time, drives the anions in the opposite direction toward the anode.

When we insert an ion exchange membrane made of cation selective resins, it will block the flow of anions and water molecules … only cations will be able to pass through to the other side.

When we insert another ion exchange membrane, this time made out of anion selective resins, it will block the flow of cations and water molecules. Only anions will be able to pass through to the other side.

This configuration of membranes and electrodes forms the framework of a CEDI module.

This process is limited however, by the slow speed at which ions move through water. In effect, the low conductivity of water impedes ion removal.  In other words, as the product compartment water becomes more and more pure, the electrical resistance of this water increases more and counters the effect of the electrical field.

Ionpure CEDI technology solves this problem by sandwiching a mixture of cation and anion selective resins between the two membranes. The large surface area now offered by the resin beads effectively eliminates the ion diffusion resistance and allows the ions to move freely even in ultrapure water solutions.

The surface of the resin beads acts as a conductive path … efficiently acting as a bridge for the ions to move quicker toward the membrane surface faster than if they were in water alone.

Taking a step back to look at how a Ionpure CEDI module is constructed, we can see that if we move the electrodes farther apart and continue to add resin beads sandwiched between the cation and anion selective membranes; we create a series of water purification compartments … alternating with compartments where the ions are concentrated.

As feedwater is pumped into the system, it is diverted into separate compartments mainly the concentrating compartment, and the purification or dilute compartment.

These water streams remain separated throughout the process because only ions can pass through the membranes.

Ions migrate and accumulate in the concentrating compartments where they are washed away in to the reject stream.  The water leaving this compartment contains a concentration of ions approximately 10 to 20 times higher than the original feed water. This water may be drained, recycled, or reclaimed for further treatment.

At the top of the purification compartments the ion concentration is at its highest. Here the surface of the resin beads acts as a conductive path, effectively moving the ions to the membrane.

At the lower end of the purification compartments, where the ion concentration has been reduced to the “parts per trillion” level, the electric field becomes concentrated between the resin beads and the surrounding water. When this localized voltage potential exceeds approximately 8/10 of a volt, an electro-chemical reaction occurs and water molecules are split into hydrogen and hydroxide ions also which are essentially acid and caustic.

The acid and caustic generated in the module regenerate the resin beads by replacing other trace ions remaining. The attachment of hydrogen and hydroxide ions to the resin beads is exactly what happens to resin beads when acid and caustic are used for regeneration in conventional deionization systems.

As a result, Ionpure CEDI Systems do not need chemicals for regeneration … the electric potential does all the work.  You essentially have a worker and polisher combined into one unit which constantly regenerates. 

And, Ionpure CEDI Systems are more effective than other electrodeionization systems when it comes to removing dissolved materials such as salts, acids and bases, as well as weakly ionized materials such as dissolved organics, silica, boron and carbon dioxide. This continuous regeneration process also eliminates pH shock and greatly extends the life of the resins.

Through the Ionpure name, Siemens continues to innovate and offer state of the art water technologies to OEMs worldwide.

top of page
Print
Contact Us

More Information

CEDI Technologies
Ionpure Technologies

Sign up for our FREE newsletter.
First Name:
Email:
We respect your privacy and will never sell or rent our subscriber list.
© Siemens AG 2011 - Water Technologies
Corporate Information | Privacy Policy | Terms Of Use | Digital ID